• Products and Partners
    Products and Partners
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
Member's Forum Expected output voltage of XNOR gate
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 631 subscribers
  • Views 840 views
  • Users 0 members are here
Related

Expected output voltage of XNOR gate

Andrew J
Andrew J over 7 years ago

Hi,

 

I have a TI SN74HC266 XNOR gate.  If I pull two inputs high (4.9v) then the output should be high - what I'm seeing is 2.6V.  Is this right?  I may not be asking this the right way: basically, I'm trying to compare two inputs are either both high or both low and in either case, I want a high output to feed into a SN74HC08 AND gate.  I've checked the voltages on the XNOR pins and they are indeed high, but the corresponding output for that gate is 2.6v - I don't think that's enough to pull my AND gate high (at least it's output given 2 inputs at 2.6V is 0V.)  I've also checked the XNOR where the two input pins are 0V and the output pin is also 2.6V.

 

I can't tell from the data sheets if this is right, although I struggle to understand these in detail at the moment. 

 

Thanks

 

Andrew

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 7 years ago

    You may have trouble with the HC chip driving the input to the next stage.

    Add a 1k ohm pull up resistor to the HC output pin. That should help pull the output to 5v.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 7 years ago

    You may have trouble with the HC chip driving the input to the next stage.

    Add a 1k ohm pull up resistor to the HC output pin. That should help pull the output to 5v.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gdstew
    gdstew over 7 years ago in reply to DAB

    The 74HC266 should have no problem driving a single 74HC08 input. The spec sheet says it is capable of driving up to 10 LSTTL loads. However it does use open drain

    outputs and so it does as you suggest need a pull up resistor on the output pin. Since it is driving single HC input, a 4.7K Ohm resistor would be better.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 7 years ago in reply to DAB

    Thanks Dab, that's all it needed.  I'm using a number of HC chips in the overall circuit and not needed pull up resistors to drive inputs down the chain (until I reached the 266) but I'm now measuring 4.9v on the output pins.  Something to file in my brain for the future. 

     

    Thanks again, I really appreciate it.

     

    Andrew