• Products and Partners
    Products and Partners
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
Member's Forum Need Advice About A Roadtest: Amber Pi Design Kit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 633 subscribers
  • Views 1705 views
  • Users 0 members are here
Related

Need Advice About A Roadtest: Amber Pi Design Kit

rscasny
rscasny over 7 years ago

Greetings. I wanted to get the advice of any top member regarding a roadtest I am getting ready to launch.

 

Let me start by saying, most roadtests begin with a meeting with the sponsor who indicates an interest in sponsoring a roadtest. My boss gives a high level view of the roadtest program, and then I fill in the details, schedules, gathering information, etc. One of the things we always point out is that the products we roadtest have to be global (they can be used in N/SA, Europe, Asia, etc.)image

 

I met with WURTH ELEKTRONIK about its Amber Pi Design Kit. AMBER PI is an expansion board for the Raspberry Pi 3B that gives the Pi a sub-1GHz RF interface. The included sensors (temperature, humidity, pressure, motion) and RF dongle which runs as remote station for the AMBER PI.

 

It seemed like a good product to roadtest. It has an IoT angle, and it seemed like a product that would appeal to both makers and professionals alike. As usual, the sponsor sends me the kits so we can ship them out to the roadtesters. Well,when I opened the box, I soon learned all the kits were for use at 868MHZ (Europe) only. I didn't see that as a problem because often times there are separate part numbers for a 915MHZ product and an 868MHZ product. This time, however, there was not one for 915MHZ. I contacted the tech support line which said : "yes, unfortunately the Amber Pi is only available with the 868MHz RF module." This poses a problem since I need to open the roadtest to North America, at the very least.

 

After some quick research, I see that while the company does not make an Amber Pi with a 915MHZ radio module installed, it does sell aimage

915 MHZ radio module separately. So the radio module would need to be swapped out.

 

Question In Need of Advice

I could very well purchase some 915MHZ radio modules and provide them to the North America roadtesters. So, they would have to swap out the radio modules. I guess if this was a quick pull out/plug in task, I wouldn't be writing this discussion. But it appears that the module is soldered in. I took a close up picture of it (pictured below) for you to see. If I'm wrong, say the word. End of story.

 

But if it requires to be desoldered/soldered, then I am somewhat concerned for a couple of reasons:image

 

-- it changes the nature of the roadtest to include the modification task instead of just focusing on the rapid prototyping capability

--What if there is damage to the radio module during the swap out.

--The swap increases the complexity of the roadtest to the point where it is possible that a roadtester may not complete the roadtest/review

 

Now, I guess I could request from the company to custom build 915MHZ versions. Moreover, since they sell it with a separate 915MHZ radio module, perhaps the swapout should be roadtested to see if it is as easy to do as is implied by the supplier tech support line.

 

So, I am looking for some advice. I want to make sure the roadtest is fair and straightforward for both the supplier and the roadtester.

 

Any comments you have would be appreciated.

 

Randall

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 7 years ago

    I don't think this is a task you should leave to the reviewers.

     

    On the one hand, it may be nice to see how "easy" such a task will be, but on the other, there is a good deal of risk. Just looking at the board, I don't think it's going to be an easy road to desolder and resolder the module. For one thing, the through-hole header pin connections are so close to the module that it's going to be a pain to try and heat up the module without melting the plastic at the bottom of the pins. You'd also need a decent amount of equipment - an under-board heater and a hot air gun look to be necessary and I've only got one of the two (the hot air gun) so it's more than likely that I'd roast the top side of the module coming out and perhaps that of the module going in. That might kill the module or an inadvertent bump may dislodge some support components (e.g. antenna matching components). While the pads are castellated, which would in-theory mean that it can be soldered without hot air ... the closeness of the through-hole headers would mean that it would be hard to get the iron at the right angle to do it - assuming you had a fine-enough tip. Thus it would be best to do it with hot air, solder paste (or solder and flux) with the same issues noted before.

     

    I would suggest either the vendor start selling modules with the 915MHz modules pre-populated and then review them, review only the 868MHz modules in EU countries only. If somewhat daring, perhaps request boards without any modules populated and have the modules separately supplied with the RoadTester to populate at their own risk (expect some failures).

     

    There's also the question if the modules are software-compatible - while they may be footprint compatible, the 868MHz band has a different amount of bandwidth (and consequently, different number of channels) available. If the software does not correctly identify the module and program it properly, there's a chance that the correct module still will not operate properly?

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 7 years ago

    I don't think this is a task you should leave to the reviewers.

     

    On the one hand, it may be nice to see how "easy" such a task will be, but on the other, there is a good deal of risk. Just looking at the board, I don't think it's going to be an easy road to desolder and resolder the module. For one thing, the through-hole header pin connections are so close to the module that it's going to be a pain to try and heat up the module without melting the plastic at the bottom of the pins. You'd also need a decent amount of equipment - an under-board heater and a hot air gun look to be necessary and I've only got one of the two (the hot air gun) so it's more than likely that I'd roast the top side of the module coming out and perhaps that of the module going in. That might kill the module or an inadvertent bump may dislodge some support components (e.g. antenna matching components). While the pads are castellated, which would in-theory mean that it can be soldered without hot air ... the closeness of the through-hole headers would mean that it would be hard to get the iron at the right angle to do it - assuming you had a fine-enough tip. Thus it would be best to do it with hot air, solder paste (or solder and flux) with the same issues noted before.

     

    I would suggest either the vendor start selling modules with the 915MHz modules pre-populated and then review them, review only the 868MHz modules in EU countries only. If somewhat daring, perhaps request boards without any modules populated and have the modules separately supplied with the RoadTester to populate at their own risk (expect some failures).

     

    There's also the question if the modules are software-compatible - while they may be footprint compatible, the 868MHz band has a different amount of bandwidth (and consequently, different number of channels) available. If the software does not correctly identify the module and program it properly, there's a chance that the correct module still will not operate properly?

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Fred27
    Fred27 over 7 years ago in reply to Gough Lui

    I'd have to agree that desoldering this without damaging the headers isn't an easy task. It's certainly possible, but not easy.