• Products and Partners
    Products and Partners
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
Member's Forum Need Advice About A Roadtest: Amber Pi Design Kit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 633 subscribers
  • Views 1695 views
  • Users 0 members are here
Related

Need Advice About A Roadtest: Amber Pi Design Kit

rscasny
rscasny over 7 years ago

Greetings. I wanted to get the advice of any top member regarding a roadtest I am getting ready to launch.

 

Let me start by saying, most roadtests begin with a meeting with the sponsor who indicates an interest in sponsoring a roadtest. My boss gives a high level view of the roadtest program, and then I fill in the details, schedules, gathering information, etc. One of the things we always point out is that the products we roadtest have to be global (they can be used in N/SA, Europe, Asia, etc.)image

 

I met with WURTH ELEKTRONIK about its Amber Pi Design Kit. AMBER PI is an expansion board for the Raspberry Pi 3B that gives the Pi a sub-1GHz RF interface. The included sensors (temperature, humidity, pressure, motion) and RF dongle which runs as remote station for the AMBER PI.

 

It seemed like a good product to roadtest. It has an IoT angle, and it seemed like a product that would appeal to both makers and professionals alike. As usual, the sponsor sends me the kits so we can ship them out to the roadtesters. Well,when I opened the box, I soon learned all the kits were for use at 868MHZ (Europe) only. I didn't see that as a problem because often times there are separate part numbers for a 915MHZ product and an 868MHZ product. This time, however, there was not one for 915MHZ. I contacted the tech support line which said : "yes, unfortunately the Amber Pi is only available with the 868MHz RF module." This poses a problem since I need to open the roadtest to North America, at the very least.

 

After some quick research, I see that while the company does not make an Amber Pi with a 915MHZ radio module installed, it does sell aimage

915 MHZ radio module separately. So the radio module would need to be swapped out.

 

Question In Need of Advice

I could very well purchase some 915MHZ radio modules and provide them to the North America roadtesters. So, they would have to swap out the radio modules. I guess if this was a quick pull out/plug in task, I wouldn't be writing this discussion. But it appears that the module is soldered in. I took a close up picture of it (pictured below) for you to see. If I'm wrong, say the word. End of story.

 

But if it requires to be desoldered/soldered, then I am somewhat concerned for a couple of reasons:image

 

-- it changes the nature of the roadtest to include the modification task instead of just focusing on the rapid prototyping capability

--What if there is damage to the radio module during the swap out.

--The swap increases the complexity of the roadtest to the point where it is possible that a roadtester may not complete the roadtest/review

 

Now, I guess I could request from the company to custom build 915MHZ versions. Moreover, since they sell it with a separate 915MHZ radio module, perhaps the swapout should be roadtested to see if it is as easy to do as is implied by the supplier tech support line.

 

So, I am looking for some advice. I want to make sure the roadtest is fair and straightforward for both the supplier and the roadtester.

 

Any comments you have would be appreciated.

 

Randall

  • Sign in to reply
  • Cancel
Parents
  • colporteur
    colporteur over 7 years ago

    It appears my response might be late to your game.

     

    I see the problem as an exercise in managing risk. My take is that you define the RoadTest options and let the vendor decide what works for them.
     

    RoadTest restricted to the markets supported by the equipment without modifications.

    RoadTest expanded markets only if equipment can be supplied by vendor.

    RoadTest expanded market with equipment modified on delivery.
     

    My reasoning is taking the perspective that the RoadTest is a supplier, that is responsible for providing results within specified parameters. Depending on what option is selected the specified parameters change. If you decide, you assume all the risk.
     

    It appears from following the comments regarding RoadTest applicant selection, that you report back to the vendor on the results of RoadTest. I seem to recall missing RoadTests is a poor performance indicator that vendors frown on.
     

    Speaking from the Element14 community, I believe there are RoadTesters capable of handling the modification successfully. You want to sell the capabilities of the option  but it does increase the risk to a poor performance indicator. You can limit the exposure by limiting the number of outside of Europe RoadTest.
     

    Depending on the parameters of the RoadTest (i.e. option) there is varied risk. How do you manage the risk and still provide the vendor the RoadTest results? You need to clearly define the risks for each option. You still have the risks but you transfer that risk outcomes to the vendor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 7 years ago

    It appears my response might be late to your game.

     

    I see the problem as an exercise in managing risk. My take is that you define the RoadTest options and let the vendor decide what works for them.
     

    RoadTest restricted to the markets supported by the equipment without modifications.

    RoadTest expanded markets only if equipment can be supplied by vendor.

    RoadTest expanded market with equipment modified on delivery.
     

    My reasoning is taking the perspective that the RoadTest is a supplier, that is responsible for providing results within specified parameters. Depending on what option is selected the specified parameters change. If you decide, you assume all the risk.
     

    It appears from following the comments regarding RoadTest applicant selection, that you report back to the vendor on the results of RoadTest. I seem to recall missing RoadTests is a poor performance indicator that vendors frown on.
     

    Speaking from the Element14 community, I believe there are RoadTesters capable of handling the modification successfully. You want to sell the capabilities of the option  but it does increase the risk to a poor performance indicator. You can limit the exposure by limiting the number of outside of Europe RoadTest.
     

    Depending on the parameters of the RoadTest (i.e. option) there is varied risk. How do you manage the risk and still provide the vendor the RoadTest results? You need to clearly define the risks for each option. You still have the risks but you transfer that risk outcomes to the vendor.