Table of contents
Abstract
I was looking for a way to make painting more interesting in availability of light and in complete darkness. The only requirement is that the painting should be intresting.
Project
Painting looks beautiful on wall but imagine painting with some section highlighted with LED light. This improves the interest of painting

Story
My wall was looking ugly. I want to add painting to the wall which does not only looks beautiful in Light but also looks beautiful without light and should also work as a night lamp for dark places. So, I figured out LED painting is the first and last choice for it.
Construction:-
tools required
scissor:-

transparent tape:-

Led string Light:-

Wooden tray:-

painting printout:-

Making the project
Stick the LED string light on the back side of the painting. While doing it stick the LED in those section of the painting which needs to be highlighted by LED as shown in the picture bellow

Switch on the LED and than stick the painting on the front of the wooden box using cello tape as shown bellow. the back strip will be used for hanging on the screw of the wall.

you project is complete.
bellow video shows how the project looks on the wall with and without light.
video with light off