Choo Choo Go Stick

Table of contents

Choo Choo Go Stick

Abstract

Modify battery operated Christmas train engine so my 4 year old grandson can make it go and stop - all by himself.

For many of us, there is a magical bond between Christmas and toy trains. One of the few déjà vu moments in my life was about a train set that I received for Christmas one year. My Dad got a Christmas train quite late in life – and was never able to part with it, even when he stopped decorating for Christmas. Looking back, it was probably something that he had wanted as a child - but he grew up dirt poor. And then he was too grown up for a kids toy. I'm glad that he finally got his train before he passed.

image

I wanted my grandkids to experience the magic of a Christmas train – so I bought one – before Dad passed – because he wasn't going to part with his. I asked – and got the Grumpy Cat look as my reply.  Hey!  Okay!  I crossed the line. Laughing  My train isn't as cool, but mine has a movie theme. Joy

image

You know... the only problem with most of these trains is they are either ON or OFF. Sure there are model railroad sets, but you don't hand one of those over to a four year old. Or a six year old.
So the kids either just get to watch – BOO! No fun there. OR... you use the kind pictured above and you're trying to put an engine on the tracks while it's running – and then attach some cars. It's painful to watch – or participate in.

What? Put it on the track and then flip the switch?

GREAT PLAN! Have you ever tried that in real life with a small child?  Even the older kids struggle.

Herein is the basis for my project. Add a Start/Stop switch to the affordable battery powered Christmas train that a small child can operate – with the train already on the tracks. And it needs to be minimally invasive so the Christmas train still looks like a train and not scrap wire on wheels. And it needs to run on 3VDC – since the train is powered by two D-cell batteries.

My initial circuit plan was to use a capacitive touch switch. Space is very limited within the train so I was trying not to go the “microcontroller and relay” route.  While looking for a way to integrate the capacitive switch, I stumbled on a latching switch module based on the MEM2313 P-channel MOSFET.  The capacitive modules that I have go high when touched and this module is momentary active low.  PERFECT!  Plan B!
If you watched the video, you already know that I went with magnetic reed switches - but to a small child... THEY are in control.  How it is achieved is immaterial - to them.

BEFORE
image     image

Pretty simple.  Flip the switch and it runs.

DURING
image

Parallel magnetic reed switches hot glued into the corners of the cab.

image

The control module.  Dime added for scale.  And its wiring diagram below.

  image

FINISH PROJECT

image

A few extra wires but still clean.

NEW SCHEMATIC

image

I added the diode for circuit protection.  When the grandson pushes the engine across the floor, it doesn't matter that the switch is OFF.  The light still lights - because the motor is also a permanent magnet generator.
And sometimes... everything with wheels is a Matchbox car.

CONCLUSION

I'm happy with the outcome but even more so with the shift to the magnetic switches.  Whether it's a wand or a whacking stick, every kid gets a giggle out of smacking a moving toy.  It's even more magical if it starts or stops doing something because of it.  Think of it as entry level training for percussive adjustment repair techniques.  For most of this train's life, it has been running into Hot Wheels, Matchbox cars, it's own cars... I don't think whacking it with a magnet on a popsicle stick is going to faze it.
Merry Christmas.  Happy holidays.  Happy New Year! Relaxed

Attachments

References

Switch Module:  https://www.amazon.com/dp/B07NYQRWSZ?ref=ppx_yo2ov_dt_b_fed_asin_title

Category : project
Parents Comment Children
  •  Great question.  I suppose I just took the path that I understood.  I wanted to use the capacitive touch switches I already had - but output was only active when touched.  So I needed a latching device - that would work on 3VDC - in a small space.  I found one that could be delivered just after Christmas - while the grandkids and I were still on holiday break/vacation.  What does it take to make that device work?  Active low, not active high like the touch sensors.  Out they go.  What will work?
    I look back at projects like these and laugh at my "quality decisions".  Was it the best decision?  Ah... maybe?  Like some, I can suffer from analysis paralysis.  This path got the project built. Relaxed

  • I've experienced your "quality decisions" dilemma and defining best:) I've also ran the gambit of needing a HIGH but having a LOW. 

    image

    I've also used capactive touch switches. I recently discovered the A & B jumper on these devices, I bought a few years ago, allow me to change the output. Who knew:)

  •   Relaxed  I immediately checked mine out.  Thumbsdown  No selection jumper on the boards I have.  Mine also uses the TTP223B chip. I would have to use some bodge wires to make it work.
    Credit to the e14 Community - I actually read the chip datasheet to figure out what it would take to do it.  ThumbsupJoy

    I originally bought the touch sensors for an iambic morse code "key".  Cool in concept.  Poor in execution.  The side of the index finger just wouldn't reliably activate the touch sensor - so... operator error.  I'm sure that I'll find a use for the sensors (maybe). Laughing