Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs 1 - Introduction of a member of the posse, and some actual electronics stuff.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mr_widget
  • Date Created: 31 Jan 2013 11:04 PM Date Created
  • Views 432 views
  • Likes 1 like
  • Comments 0 comments
  • powah
  • humph
  • posse
  • members_featured_project
Related
Recommended

1 - Introduction of a member of the posse, and some actual electronics stuff.

mr_widget
mr_widget
31 Jan 2013

This is a picture of my muse, Mr. Humphrey Lyttleton Katz or Chairman Humph, for short.

image

image

He is saying here, "Go away. You're so boring.  Get over yourself."

Actually Humph is probably the neediest cat I ever had, in his own weird way.

Enough about Humph.

 

Here is a project I have been working on, of late:

 

imageimage

 

This one is called the Powah.  It is just a little on/off toggle with an indicator LED.  It is designed to mount on one end of my breadboard, so as to reduce the wear and tear caused by excessive insertions of power bus leads.  The board is approx 1 cm^2.

imageimage

Pretty nifty, eh?  I searched around and the closest thing to this is a power switch from Pololu, which I did not find that interesting (too large and did not have the 100-mil form factor. Here is a schematic:

 

image

image

It is very simple, as you can see.  The main limitation is that the power for the IC is tied to the input, so the DC level is limited to 6V.  Turned on, the current loading from the Powah is 3.06mA. Turned off, the loading is unmeasurable with my crusty old B&K multimeter.  If I can sell enough of these, and perhaps some other ones I am working on I can spring for a nice Fluke one.

 

Here is an alternative design I have been noodling right now:

image

image

The main advantages here are:

 

The MOSFETS are complementary and on the same die, so they are matched.  And they are much beefier so the current passage has more safety (I would be comfortable passing at least 2A through this device).

 

The Zener limits the gate power supply to 5.1V, so the input switching can go all the way to the breakdown limit of the P-channel MOSFET, which is 20V.

 

Turning on the switch requires only a short button press, while turning off the switch requires a longer button press, as a fail-safe.

 

The inherent hysteresis of the Schmitt front-ends on the gates means that the reset signal on the second pair requires a time interval before the latch signal is active.  This is a free way to debounce the circuit.

 

The main disadvantages are the increased complexity and part-count requires the board real-estate to also increase.  I have managed to fit the whole works on a 0.8 x 0.5 inch board.  There are, to my knowledge, anything like a 74LVC2G7002 device out there.  I wish there were, as I think I could fit 2 SO8's better than the SO14.

 

Here is a 3D rendering of what that board is likely to look like:

image

 

image

image

Anyway, enough of my blather.  'Till next time.image