Products
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
Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs A Small Simple Robot Arm : Part 2 Initial Software Implementation
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 31 Jan 2020 3:36 PM Date Created
  • Views 2048 views
  • Likes 9 likes
  • Comments 14 comments
  • nano
  • robot arm
Related
Recommended

A Small Simple Robot Arm : Part 2 Initial Software Implementation

dubbie
dubbie
31 Jan 2020

Having constructed the small 4 degree of freedom (4 DOF) plastic robot arm, similar to the MeArm,  ( A Small Simple Robot Arm : Part 1 Mechanical Construction  ) I have now added a Nano controller and some simple software.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

For this initial software I have not used the Servo library but instead written my own PWM generation for the micro servo motors. I did this for two reasons; first I wanted to have complete control over the servo motors rather than relying on someone else's library and second to reduce the drain on the battery. Using the Servo library results in the servo motors being driven all the time, which is good for position control but bad for power consumption. As I generally use AA batteries to power most of my projects then reducing battery drain is important, especially during the initial getting going and testing periods. I may well change to using a servo library in later software once I am happy with everything else.

 

RC servo motors, including micro servo motors, use much the same PWM structure to operate. Every 20 ms there is a pulse of at least one ms but no longer than 2 ms. Altering the pulse width from 1 ms (equivalent to 0 degrees on the servo motor shaft) to 2 ms (equivalent to 180 degrees on the servo motor shaft) enables the angle of the servo motor to be controlled very easily from a microcontroller such as the Nano.

 

Below is the function I have written to produce this waveform, without using any timers or interrupts.

 

void myservo(int select_servo, int servo_value)

// servo_value must be between 0 and 2000
{

  int index;

  if (servo_value < 0)
    servo_value = 0;
  if (servo_value > 2000)
    servo_value = 2000;
   
  for (index = 0; index < 30; index++)
    {
      digitalWrite(select_servo, HIGH);   // Start the servo pulse
      delayMicroseconds(500);             // Basic pulse period part
      delayMicroseconds(servo_value);     // Additional delay for servo position
      digitalWrite(select_servo, LOW);    // End the servo pulse.
      delayMicroseconds(2000 - servo_value);
      delay(18);                          // wait for the pulse space
    } /* for */
}

 

I create a pulse of at least 1000 us which is then extended by up to a further 1000 us to provide accurate control of the pulse and hence (hopefully) the servo motor angle, with a 18 ms delay, the space delay, at the end. It is not particularly clever but it does work.

 

I decided to use a serial text user interface as this provides the options of using the Serial Monitor built into the Arduino IDE or using a Bluetooth serial communications link to a mobile phone, using an App called BlueTerm. I have used this App before, it is not the best as it can be a bit unreliable with the Bluetooth link, but it is simple. At the moment I am using the Serial Monitor within the Arduino IDE.

 

Arduino does not provide a comprehensive ASCII character input function, just the Serial.read() function, which is for individual characters so I have modelled my User Interface on single character entry. To avoid crashing the input I treat all inputs as ASCII characters instead of integers and then use a switch statement to convert to integers. It is a bit clunky but it it is simple and it does work. Below is an example of selecting the Base rotation. I allow angles to be multiples of 10 degrees so the selection is from 0 degrees to 180 degrees (the number 0 to the letter I).

 

void Base(void)

{

int base_select;
int base_angle;

  base_angle = 0;
  base_select = 0;
  Serial.println("Base Servo Selected ");
  Serial.println("Select Base Angle ");
  Serial.println();

  Serial.println("0 degrees   : 0 ");
  Serial.println("10 degrees  : 1 ");
  Serial.println("20 degrees  : 2 ");
  Serial.println("30 degrees  : 3 ");
  Serial.println("40 degrees  : 4 ");
  Serial.println("50 degrees  : 5 ");
  Serial.println("60 degrees  : 6 ");
  Serial.println("70 degrees  : 7 ");
  Serial.println("80 degrees  : 8 ");
  Serial.println("90 degrees  : 9 ");
  Serial.println("100 degrees : a ");
  Serial.println("110 degrees : b ");
  Serial.println("120 degrees : c ");
  Serial.println("130 degrees : d ");
  Serial.println("140 degrees : e ");
  Serial.println("150 degrees : f ");
  Serial.println("160 degrees : g ");
  Serial.println("170 degrees : h ");
  Serial.println("180 degrees : i ");

  Serial.println();
  base_select = ' ';
  while (Serial.available() < 1)
    {
      delay(10);
    } /* while */
  base_select = Serial.read(); 
  switch (base_select)
    {
      case '0' : base_angle = 0;   break;
      case '1' : base_angle = 10;  break;     
      case '2' : base_angle = 20;  break;
      case '3' : base_angle = 30;  break;
      case '4' : base_angle = 40;  break;
      case '5' : base_angle = 50;  break;
      case '6' : base_angle = 60;  break;
      case '7' : base_angle = 70;  break;
      case '8' : base_angle = 80;  break;
      case '9' : base_angle = 90;  break;
      case 'a' : base_angle = 100; break;
      case 'b' : base_angle = 110; break;
      case 'c' : base_angle = 120; break;
      case 'd' : base_angle = 130; break;
      case 'e' : base_angle = 140; break;
      case 'f' : base_angle = 150; break;
      case 'g' : base_angle = 160; break;                 
      case 'h' : base_angle = 170; break;                  
      case 'i' : base_angle = 180; break;               
      default  : Serial.println("Unknown Command ");
                 base_angle = 90;
                 delay(1000);             
    } /* switch */

 

There are similar functions for the Shoulder(), Arm() and Grip() servos, although the gripper only has three positions; open, middle, closed. The main loop then just cycles through to select which servo motor is to be changed (Base, Shoulder, Arm, Gripper) and uses another switch statement to activate the appropriate joint function, see below.

 

 

while (1)
  {
    Serial.println("Small robot Arm " );
    Serial.println("Dubbie Dubbie : Just for Fun " );
    Serial.println(" 21st Jan'20 ");
    Serial.println();
    delay(500);

    Serial.println("Select Servo  ");
    Serial.println("Base     : 1 ");
    Serial.println("Shoulder : 2 ");   
    Serial.println("Arm      : 3 ");
    Serial.println("Grip     : 4 ");
    Serial.println();
    int value = ' ';
    while (Serial.available() < 1)
      {
        delay(10);
      } /* while */
    value = Serial.read();

    switch (value)
      {
        case '1' : Base();
                   break;
        case '2' : Shoulder();
                   break;
        case '3' : Arm();
                   break;
        case '4' : Grip();
                   break;
        default  : Serial.println("Unknown Command "); delay(1000);             
      } /* switch */
    delay(1000);
     
  } /* while */

 

I am quite happy with what I have produced so far but I am thinking of making it better, if I can. The servo motor movements are fairly jerky as they try to move from the current position to the next position as quickly as possible, without any acceleration or deacceleration. I would like to see if I can make these movements much smoother which I believe may be called servo easing. I'm not sure what the trigonometric function is, some sort of sine or cosine I think, which I could put into a lookup table and then somehow combine with the distance to be moved.

 

Dubbie

  • Sign in to reply

Top Comments

  • luislabmo
    luislabmo over 6 years ago +5
    Hello Dubbie, nice update!. I believe a couple of loops and some ascii conversions could have saved you a lot of coding when printing the menu and also when translating the input to degrees. Luis
  • dubbie
    dubbie over 6 years ago in reply to luislabmo +4
    Luis, I agree, with a bit of thought I could have made it more efficient but time was short and I wanted some software that was easy to understand, most likely to work and easy to amend/extend. Then, once…
  • shabaz
    shabaz over 5 years ago in reply to dubbie +4
    Hi Dubbie, You might find that depending on the position of where one servo is, it affects the amount of motion available to the other servo, due to the linkages affecting them. Not sure. Anyway, if you…
  • dubbie
    dubbie over 5 years ago in reply to beacon_dave

    Dve,

     

    Looks like a nice industrial style robot.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 5 years ago

    This robot arm on YouTube may be of interest:

    fischertechnik 6-Achs-Roboterarm RS 816 - YouTube

     

    I spotted in the latest ft:pedia magazine:

    https://www.ftcommunity.de/ftpedia/2021/2021-1/ftpedia-2021-1.pdf

    where there is more information.

    (There is also an article there on mecanum and omniwheels amongst other things.)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 5 years ago in reply to dubbie

    Dubbie,

     

    Part way through the series I became disillusioned - there was little hands on electronics work, mostly just plugging together the modules that came with the magazine. There was little explanation of how the modules worked and no schematics. To make matters worse, the build quality of some of the modules was pretty poor.

     

    Can't remember how much I spent on it (ouch), but when I resurrected it back in 2015, I had a lot of fun with it and learned a lot,

     

    Neil

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 5 years ago in reply to dubbie

    Gene,

     

    I missed a word out, I meant buy something if I need it.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 5 years ago in reply to genebren

    Gene,

     

    A good concept. Perhaps a bit too complicated for me, maybe I'll just something similar should I need to. Much easier.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>