Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Aluminum PCB Heat Transfer Basics for LED Applications
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 11 Dec 2009 8:24 PM Date Created
  • Views 1814 views
  • Likes 0 likes
  • Comments 0 comments
  • resistance
  • aluminum_pcb
  • conduction
  • pcb_design
  • led
  • circuit_board_manufacturer
  • conductivity
  • convection
  • themal_management
  • heat_transfer
Related
Recommended

Aluminum PCB Heat Transfer Basics for LED Applications

e14 Contributor
e14 Contributor
11 Dec 2009

Basics of Heat Transfer

To understand the heat transfer properties of thermal interface materials (TIMs) we need to understand the meaning of thermal conduction, convection and resistance.  The following is a sneak peak from Clemens Lasance's Thermal Interface Material Basics for Electronic Engineers. Clemens recently presented this information in relation to the role of the PCB in Thermal LED Applications at the MCPCB Design and Fabrication webinar.

 

Conduction

The notion of thermal conduction is not very old. Biot (1804) and Fourier (1822) were the first to quantitatively study the heat flow through a piece of solid material. Fourier observed that the heat flow q was proportional to the temperature difference ΔT over the test piece, proportional to the cross sectional area A of the bar, and inversely proportional to the length or thickness ℓ., known as Fourier’s law:

                                                                (1)

The proportionality constant k is called the thermal conductivity in W/mK. It is a material property and a measure for the ability of a material to conduct heat. The range for engineering materials is from air (0.03W/mK), via plastics (0.2 W/mK), glass (1 W/mK), aluminum PCB board (200 W/mK) to copper board (400 W/mK). Typical TIM values cover the range 0.4-4 W/mK.

 

Convection

The heat generated in an electronic device is usually transported by conduction to a heat sink or an area where the heat is transferred to a fluid which is called convection. The fluid can be a gas such as air, or a ‘real’ fluid such as water. As a result, the convection heat is proportional to the area A and the temperature difference between the wall and the main stream flow:

                                                                   (2)

This equation is commonly known as “Newton’s Cooling Law”; however, it should be realized that it is neither a law nor was it derived by Newton.  In this equation, the proportionality coefficient h is called the heat transfer coefficient in W/m2 K. As a rule-of-thumb, take for natural convection h=10 W/m2 K and for fan-driven forced convection h=50 W/m2 K.

 

Resistance

The last term to discuss shortly is the thermal resistance. In a DC electrical circuit, Ohm’s law describes the relations between the voltages and the currents. It states that a voltage difference over a resistor causes an electrical current, which is proportional to the voltage difference: ΔV = I * R. 

 

In steady state heat transfer, a temperature difference causes a heat flow which is proportional to the temperature difference as is seen in equations (1,2). Both equations can be written in the form ΔT = q * Rth, with Rth the thermal resistance (also commonly noted as R when there is no chance for misreading it as an electrical resistance). This is analogous to Ohm’s law. In both the electrical and the thermal case we observe that a driving force exists (either voltage difference or temperature difference), which causes a flow (of current, or of heat) over a resistor.

 

The thermal resistance per unit area  is equal to the ratio between thickness t and thermal conductivity k and is often used to allow for a direct comparison of the heat transfer performance of commercially available TIMs.

 

About Clemens Lasance

Clemens is a former Principal Scientist Emeritus with Philips Research, the Netherlands,  with a 30 year + focus on thermal management of electronic systems.  He is now a consultant for Somelikeit Cool, contact info: lasance@onsnet.nu

 

About Saturn Electronics Corporation

Aluminum PCB Manufacturer Saturn is a top 30 domestic bare printed circuit board fabricator managing the nuances between prototype and production while providing advanced technologies such as thermal management for LED PCBs.