Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Arduino pro Mini plans
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: funinalaska
  • Date Created: 9 Sep 2014 8:54 PM Date Created
  • Views 615 views
  • Likes 0 likes
  • Comments 0 comments
  • arduino_promini
  • lighting
  • network
  • temperature
  • arduino_mega2560
  • relays
  • nrf24l01
  • home
  • automation
Related
Recommended

Arduino pro Mini plans

funinalaska
funinalaska
9 Sep 2014

Ok, so the grand plan for my house will include me networking a few Arduinos each having different but similar duties.

I am using this blog post to sort of work through my plan.

First will be my central control station. This will be an Arduino Mega.

The mega will be using a Wiznet 5100 ethernet shield for network access to the system as well as for dataloging at least that's the plan.

It will also be connected to an 8 channel relay panel which will be controlling the primary lighting on the first floor of my house.

I also plan to have a display connected to it to display temperature readings and other information both from the mega as well as from some of the remote systems.

I also plan to have an input panel of some sort, maybe a 4X4 numerical pad for input and control.

I plan to also have an NRF24L01 (If I can figure the damn things out) network communicating to my remote Arduinos.

There will also be a temperature and humidity sensor for the indoor main living area monitoring.

I will also need a IR receiver that will be receiving commands from an IR remote to control lighting and display in a similar way to the 4X4 panel.

The final piece is 4 channels of PWM for RGBW lighting control through power transistors for my living room lighting, but this MAY be on a separate satellite unit.

The remote units are one in the basement and one on the second floor. Both of these will be very similar.

Each will have an additional 8 channel relay panel for lighting

an NRF24L01 for communications with the main unit

And 2 temperature sensors, one indoor and one outdoor both will be DS18B20 units.

I would also like to have a local display on each of these so the indoor and outdoor temps can be visible locally.

And also a control panel similar to that of the main unit.

 

So it is a big project, but I think through tackling it a piece at a time I will be able to make it work.

So my next step of tackling this project is learning how to connect and program the Arduino Pro Mini

I want to be able to program and experiment with the Pro Mini units without soldering headers on to them

So I am going to try using those micro clamps that hook through a hole on a PCB.

If this doesn't work I guess I will be soldering headers on to the units.

I plan too (at least for now) program the Pro Minis with an Arduino Uno

Eventually as I build an enclosure for each portion of my home project I plan to get an ISP of some sort and have an easily accessible port to plug into for any programming updates or changes I need to make in the future.

 

I was also wondering if anyone has any experience with using bare chip ATtiny85 chips and if these chips can be used with the NRF24L01.

This is a curiosity question more than anything, just wondering if it would work.

Mainly this would be to communicate with a barebones controller that will be running and communicating back info from one or two remote sensors.

If I can't do this with the ATtiny85 I will just get more Arduino Pro Minis later.

I just ask because I have a whole bunch of the ATtinys

 

The only things I am missing from the primary system (main unit and 2 satellites) is the control interface surface.

And the lighting still needs to be installed in the house in locations and ways the wife approves of. LOL