Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Arrival and Connection
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scott.pett
  • Date Created: 18 Sep 2012 10:48 AM Date Created
  • Views 629 views
  • Likes 1 like
  • Comments 0 comments
  • monitor
  • raspberry_pi
  • 'hp
  • f1903'
Related
Recommended

Arrival and Connection

scott.pett
scott.pett
18 Sep 2012

Well, the Pi turned up a while back. Not owning an HD telly meant that a monitor needed to be found.

 

My old HP F1903 has been in use as a second screen on the iMac for some time and thankfully has a DVI port in additon to the VGA used by the Mac.

 

How hard can it be?? Cheap HDMI -> DVI-D cable from Maplin. (No such thing - its more expensive than the PI!)

 

Cheap HDMI -> DVI-D cable from Amazon then - that's better.

 

Unfortunately, a lousy picture - green lines and rubbish all over the screen...

 

Anyway - the upshot of loads of hours mucking about with the config.txt settings; reboots and using an even more ancient Phillips CRT monitor from my Atari XE days

and contrary to the instructions in Eben's new eBook manual; the following settings worked for me:-

 

# Config.txt

# Using cheap HDMI to DVI converter cable to HP F1903 Monitor

# Best mode appears to be Mode 36 (1280x1024 75Hz)

#

# HDMI type DMT

hdmi_group=2

#

# Drive is DVI Sans Sound

hdmi_drive=1

#

# The following modes are supported by the HP F1903

#hdmi_mode=4

#hdmi_mode=5

#hdmi_mode=6

#hdmi_mode=9

#hdmi_mode=10

#hdmi_mode=11

#hdmi_mode=16

#hdmi_mode=18

#hdmi_mode=35

hdmi_mode=36

#

# So we get a bit of border round the edges

#

disable_overscan=0

 

# Boosting the HDMI Signal to get rid of green line interference

# Anywhere between 1 and 7

# 2 seems to work, 3 is better in LDXE

config_hdmi_boost=3

#

 

So there you have it. A working monitor for the Pi, which I can use a t the same time as the iMac. Press the -/1 button for iMac's VGA screen and the +/2 button for the Pi's DVI display.

(Don't forget to ser the monitor to "Video Input Select/Auto Detect")