Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Atmel AT91SAM9G45 Microcontroller Datasheet
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kennyxie
  • Date Created: 6 Jan 2010 6:52 AM Date Created
  • Views 783 views
  • Likes 0 likes
  • Comments 1 comment
  • sam9g45
  • arm_development_tools
  • atmel_at91sam9g45
  • arm9
Related
Recommended

Atmel AT91SAM9G45 Microcontroller Datasheet

kennyxie
kennyxie
6 Jan 2010

This article is forwarded from Atmel, it mainly describes the delighted features of the new Atmel AT91SAM9G45 ARM9 Microcontroller which is released by Atmel in December of 2009.

 

Atmel's SAM9G45 is a high-performance eMPU with the right peripheral mix and performance characteristics to make it the ideal solution for main powered, cost-sensitive industrial applications such as industrial & building control, HVAC, POS terminals, alarm systems, printers and medical.

 

High-speed Connectivity and Intelligent User Interfaces
Combines 100 Mbps+ data rates on multiple high-speed peripherals including HS USB, Ethernet 10/100, SDIO/SDCard, MMC with advanced intelligent User Interfaces (LCD, Camera, Touch screen and audio interfaces).

 

High Performance Data Speedway
Features a processor clock running at 400 MHz and a high data-bandwidth architecture based on a 12-layer bus matrix with 37 DMA channels. Dual External Bus Interface supporting distributed on- and off-chip memory.

 

Next-generation Memories
Offers DDR2 and NAND Flash support, in addition to SDRAM and NOR Flash, with boot from NAND Flash, SDCard, DataFlashRegistered or serial DataFlash.

 

Low Power, Low Cost
Only 350µW/MHz at 400 MHz operation and 8µA backup mode. 3.3V IOs eliminate the need for external level shifters.

Attachments:
imageAtmel AT91SAM9G45 datasheet.pdf
  • Sign in to reply
Parents
  • kennyxie
    kennyxie over 16 years ago
    You can find the ATMEL SAM9G45 ARM9 Evaluation Board through the following link: http://www.embedinfo.com/en/list.asp?id=72.image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kennyxie
    kennyxie over 16 years ago
    You can find the ATMEL SAM9G45 ARM9 Evaluation Board through the following link: http://www.embedinfo.com/en/list.asp?id=72.image