Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Automate Rigol Power Supply with LabVIEW
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 5 Jan 2018 6:47 PM Date Created
  • Views 5502 views
  • Likes 4 likes
  • Comments 2 comments
  • labview
  • scpi
  • rigol
Related
Recommended

Automate Rigol Power Supply with LabVIEW

Jan Cumps
Jan Cumps
5 Jan 2018

A check-out the Rigol LabVIEW example for the DP800 series of power supplies.

image

 

I'm planning to automate the measurements on the programmable electronic load that Peter, Jon and I are designing here on element14. For that I need to control a power supply, that load and an oscilloscope.

In this exercise, I'm learning to program the Rigol DP832A, in particular enabling a channel and set it to several values repeatedly.

 

Rigol's Example

 

On Rigol's website you can find an example that controls the instrument and reads some data.

You can select a channel, set the voltage, then configure and control protection for over-voltage and over-current.

The program then measures the actual voltage and current, and logs it to time based plots.

 

I can use several of the blocks for my exercise. I'm trying to let the power supply step through a set of voltages, then do measurements on a device under test based on those voltages.

I'm not that interested at the moment in the measurement and logging features, but will check them out anyways.

 

The example program comes with the driver for the supply. You download it as a zip file.

Installing is done by extracting that archive in the [D:\Program Files (x86)\National Instruments\LabVIEW 2014]\instr.lib folder (you'll have to find your LabVIEW installation folder and adapt the path to that).

You can then find and run the example from the instr.lib\RIGOL DP800 Series\RIGOL DP800 Series.lvproj project.

image

Setting Initial Parameters

 

In this test I'll use the GUI to set the parameters before execution. When automating my setup I'll use the LabVIEW to set everything to a known state.

 

image

 

I select the instrument in the VISA resource control, select the channel and voltage.

In the lower part of the screen I set the limits of the supply and activate them.

When I press the Run arrow at the top of the screen, the LabVIEW program starts and applies all these settings. It then activates the channel.

 

image

In the background, the workflow each time uses SCPI to talk to the device:

image

... and each of those SCPI calls use a lower level state machine that talks to the supply:

 

image

 

LabVIEW lets you step through these flows. It highlights the block that's active and you can check payload.

In the example below, you see the result of selecting the channel, and enabling the over current protection. The SCPI command that combines these is being prepared just before it's sent to the instrument:

image

  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 8 years ago +1
    Nice to see some Rigol apparatus talking to other software without too many issues. The scope and waveform generator I have from them were very much into Rigol's own bespoke software and even that had…
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to three-phase +1
    I have one of their scopes and it works well with LabVIEW. I’m planning to add it to my project to do voltage measurements (I don’t have a SCPI capable meter).
Parents
  • three-phase
    three-phase over 8 years ago

    Nice to see some Rigol apparatus talking to other software without too many issues.

     

    The scope and waveform generator I have from them were very much into Rigol's own bespoke software and even that had its headaches.

     

    Kind regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 8 years ago

    Nice to see some Rigol apparatus talking to other software without too many issues.

     

    The scope and waveform generator I have from them were very much into Rigol's own bespoke software and even that had its headaches.

     

    Kind regards

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to three-phase

    I have one of their scopes and it works well with LabVIEW. I’m planning to add it to my project to do voltage measurements (I don’t have a SCPI capable meter).