Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Automating My Home
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tonyboubady
  • Date Created: 13 May 2016 7:41 AM Date Created
  • Views 996 views
  • Likes 1 like
  • Comments 2 comments
  • arduiono
  • diy home automation
  • home automation
Related
Recommended

Automating My Home

tonyboubady
tonyboubady
13 May 2016

I have decided to do a little project for my home. There is a two light domes in front gate pillars of my home, we used to switch on the light at evening time as it will get too dark, and we are too lazy to ask each other to do so on regular basis...well, my brain start to think about "How to make it automated". I did a quick code in Arduino...

 

A LDR to read the light source, a potentiometer to calibrate the trigger point to switch on the light, a set button for manual calibration, a smart button to auto calibration. I am going to use the raw ADC value of LDR and as well potentiometer value. While setting manual calibration, the potentiometer value will be the trigger point of light source, the set button stores the value of the potentiometer in variable for trigger point. the smart button is just store the current LDR value as trigger point, it's very useful to set the exact atmosphere light source reading.

 

This is the code...

 

int sensorValue, 
    calibration,
    quickCalibration,
    triggerPoint,
    setButtonState = 0,
    smartButtonState = 0;


void setup() {
  pinMode(8, OUTPUT);
  pinMode(7, INPUT);
  pinMode(4, INPUT);
  Serial.begin(9600);
}


void loop() {
 sensorValue = analogRead(A0); // ADC value from LDR
 calibration = analogRead(A1); // ADC value from potentiometer
 setButtonState = digitalRead(7);
 smartButtonState = digitalRead(4);




 if (setButtonState == HIGH) {
     triggerPoint = calibration; // Manual calibration
 }


 if (smartButtonState == HIGH) {
     triggerPoint = sensorValue+25; // Smart calibration
 }

 if (sensorValue < triggerPoint){
     digitalWrite(8, HIGH); // Output to relay
  } else {
     digitalWrite(8, LOW); // Output to relay
  }
  
 Serial.println(sensorValue);
 Serial.println(calibration);
 delay(5); 
}

 

It's just on breadboard level I have to buy a relay to handle 220V switching and power supply for MCU My first thought was to use ATTiny13A but due to it's low memory of 1KB I have to go for ATmega8-16PU

 

I will continue to update this project when it's progress...

  • Sign in to reply

Top Comments

  • spannerspencer
    spannerspencer over 10 years ago +2
    Excellent idea. I've been considering similar at my house -- it's dark around the back, but it gets a lot of rain and bad weather, so PIR lamps just don't last. I'm seeing a lot of people putting variations…
  • tonyboubady
    tonyboubady over 10 years ago in reply to spannerspencer +1
    Thanks Spanner, well, i do have the ESP8266 -01 module quite a while, just haven't put that in real use... but your suggestion for this project make me so...I will update regularly on progress of this…
  • tonyboubady
    tonyboubady over 10 years ago in reply to spannerspencer

    Thanks Spanner, well, i do have the ESP8266 -01 module quite a while, just haven't put that in real use... but your suggestion for this project make me so...I will update regularly on progress of this project...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spannerspencer
    spannerspencer over 10 years ago

    Excellent idea. I've been considering similar at my house -- it's dark around the back, but it gets a lot of rain and bad weather, so PIR lamps just don't last.

     

    I'm seeing a lot of people putting variations of the ESP8266 to use for a simple option for sending sensor data and simple GPIO actions via Wi-Fi. Maybe you could hook it up so you've got smartphone and/or computer control of your lights too? This looks like quite a nice (and very affordable) breakout board for the ESP8266: GeekcreitTm Doit NodeMcu Lua ESP8266 ESP-12E WIFI Development Board Sale - Banggood.com

     

    Either way, keep us posted on your progress!