Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Banggood Shopping
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsjawale24
  • Date Created: 24 Oct 2021 11:29 AM Date Created
  • Views 1807 views
  • Likes 0 likes
  • Comments 2 comments
  • signal generator
  • voltmeter
  • soldering station
  • instruments
  • soldering iron
  • soldering
  • tools
  • ammeter
  • multimeter
  • power meter
Related
Recommended

Banggood Shopping

rsjawale24
rsjawale24
24 Oct 2021

I'm doing some upgrades in my existing workbench. I don't have any good/powerful tools and instruments with me yet so I decided to do some shopping from Banggood.

Here's a quick look at items that I ordered.

image

 

1. A 8W USB soldering iron - USD 11.99

2. T12 soldering station - USD 21.66

3. XR2206 signal generator kit - USD 5.49

4. USB power meter - USD 7.56

5. Digital panel meter (3 pcs) - USD 8.26

 

USB Soldering Iron

 

The 8W USB soldering iron is quite handy and light weight. It comes with a handle which contains the heating element and the circuit. A fine tip for soldering, some soldering wire, a small stand with sponge and a USB cable.

I have tried the iron it works pretty well. It can work in 3 temperature modes - 330 C-350 C, 370 C- 400 C, and 430 C - 450 C.

The handle has a single switch with embedded LED to power it on/off and change the modes. I bought this for small and portable soldering work where I cannot carry my soldering station.

image

image

image

T12 Soldering station

Though I recently bought a Tenma digital soldering station, I wanted to give the T12 tips a try. After looking up on YouTube for various T12 soldering station, I came across a lot of videos on this inexpensive T12 soldering station. There are various versions - 8051 based, STM32 based and brands available for this station like KSGER, Quicko.  I found this inexpensive Quicko T12 soldering station on Banggood and decide to give it a try. I didn't go for the KSGER STM32 based ones as they were out of my budget and I already own a decent soldering station.

 

The T12 soldering station is a compact sized station, it comes with a handle, a T12-K type tip, 4 rubber pads and a tip fastener. The station does not have an inbuilt power supply and can be powered using an external 12V 3 A supply.

The main unit of the station has an OLED display and a rotary encoder for selecting menu options and setting the temperature. One the back side, it has a ON/OFF switch.

The handle is made up of plastic and has a silicone wire.

image

 

image

 

XR2206 Signal Generator Kit

XR2206 is an obsolete IC, but still there are various cheap signal generators built around this IC. I always wanted to have a signal generator and this works for most audio frequency experiments. It can go upto 1MHz only and hence is of not much use if you want to do RF projects. Another such popular signal generator IC is ICL8038 by Intersil (Now Renesas). This is a DIY kit. It comes with all the required components, knobs for the pots, a clear casing and the PCB. I'm yet to test it.

image

 

USB power meter

This tool is very useful to analyse the power consumption of USB devices. I remember seeing a similar USB meter in some video of either Electronoobs or GreatScott's YouTube channel.

This meter can measure- voltage, current, power, energy consumption, impedance and the time. All of the measured results are displayed on a colourful display. One can also save up to 9 readings in the USB itself.

image

image

 

Digital panel meter

Again, a useful instrument for use in simple projects. This panel meter can measure DC voltages and currents of up to 100V and 10A respectively. I remember seeing it in some YouTube videos and it worked pretty well. Hence, I decided to buy one for my projects. I bought a pack with 3 pieces of the meter. It has a bright and large 7 segment display of current and voltage. It also has a calibration pot on the back side.

image

I will post separate blogs for each of the products and write a review of how well they work.

  • Sign in to reply
  • rsjawale24
    rsjawale24 over 4 years ago in reply to jw0752

    Haha yes!

    Fortunately, this kit comes with an instruction manual.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 4 years ago

    Fun stuff, I have always enjoyed playing with the Chinese kits. Some of the time they don't work and this is even more fun as it is a puzzle to solve and fix. The fact that they seldom come with directions also is a fun challenge.

     

    John