Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Big Red CNC v2.0
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: binarygenius
  • Date Created: 21 Sep 2015 5:35 PM Date Created
  • Views 1353 views
  • Likes 3 likes
  • Comments 5 comments
  • cnc
  • milling
  • red
  • Big
  • router
Related
Recommended

Big Red CNC v2.0

binarygenius
binarygenius
21 Sep 2015

I have finally managed to get the rest of the aluminium for Big Red 2.0 and it is performing very well, i will be fitting it with perspex sides, MDF Spoilboard and i am now able to upgrade it to full aluminium construction with the Y Axis linear bearings upgraded to fully supported rails.

 

The beginning of a quick test of the machine using a pencil to draw Sweet Dreams with a heart ether side which i plan to engrave in some perspex and side light with a few RGB LEDS.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

End of test

This video is unavailable.
You don't have permission to edit metadata of this video.

 

i have added a vacuum system and the thing with the copper wire wrapped round next to the router is a small camera to help with alignment of the tool. i still need to get the aluminium plate for the front, back, part of the Y- Axis and all the parts for the Z-Axis milled but for now the Big Red has no problem cutting wood and plastic. i am currently running the motors at 24v 4A but i have still to fit a couple of boost converts to kick the voltage up to the max the drivers can comfortably handle of 40v 4A which will help increase the speed. i have already had the Y Axis running at 3500 mm/sec which is about 137 IPM but for testing i have been running at between 500-1000 mm/sec 19-39 IPM to make sure i dont kill it with one wrong move.

                                                                                                           

image
Isometeric view of CAD model with the perspex sides and MDF spoil board
image
Right view of CAD model
image
Isometeric view of CAD model
image
Front view of CAD model
image
Back view of CAD model
image
45×45 Extrusion Gantry on Big Red V1 for scale.
image
45×45 Extrusion Gantry on Big Red V1 from the front for scale.
image
960w 24v PSU worth over £500 that i picked up for £30 on ebay in the small hours of the morning
imageimage
I have now added fans and covers to keep the driver cool
image image
image
USB keypad used to control the machine until i build something better
image
i placed some magnets on the back to allow me to stick it to stuff
image
I have 15mm aluminium plate for the front panel but i need the motor holes machining before i fit it
image
For now i am using wooden panels
image
1.4W 445nm Laser which can be mounted to enable laser etching and cutting of thin materials
image
dust guard and vacuum system
image image
Magnetic dust shoe i made
image
the copper was temp holder while i aligned the camera
image
An old bagless hoover is being used for dust collection for now but i will be making a cyclone dust seperator at some point.
image
An old TV bracket with a shower rail bolted on so the vacuum pipe can move with the CNC
image
The Super PID router speed controller is now mounted in a nice abs     case and all the cables are now run to allow control of it from mach3
image image
E-Chain used to carry the cables
  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Very well explained post. What kind of spindle do you plan to use for milling ?
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to binarygenius +1
    Thank you Mick. Wait to see what happens further Enrico
  • DAB
    DAB over 10 years ago +1
    Nice project. What is your end use application? DAB
Parents
  • DAB
    DAB over 10 years ago

    Nice project.

     

    What is your end use application?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • binarygenius
    binarygenius over 10 years ago in reply to DAB

    well end use is only limited by my imagination. i will be making furniture for the house because flat packs never fit right and it is also accurate enough to mill things like this http://binarygenius.com/CAD/index.html using a 0.1mm engraving bit and once we get a better cutting head i want to be able to mill at least aluminum because we are 3d printing plastic parts and then using them as molds for an aluminum forge me and my son are making, then we can finish the part with the cnc. This machine will never be finished because i want to have it so i can change pullys so i can increase speed or torque and have it so i can change the head from milling to laser cutting, drag knife, large scale 3d printer or anything i can attach to it and have at least 4 axis possibly 5 image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • binarygenius
    binarygenius over 10 years ago in reply to DAB

    well end use is only limited by my imagination. i will be making furniture for the house because flat packs never fit right and it is also accurate enough to mill things like this http://binarygenius.com/CAD/index.html using a 0.1mm engraving bit and once we get a better cutting head i want to be able to mill at least aluminum because we are 3d printing plastic parts and then using them as molds for an aluminum forge me and my son are making, then we can finish the part with the cnc. This machine will never be finished because i want to have it so i can change pullys so i can increase speed or torque and have it so i can change the head from milling to laser cutting, drag knife, large scale 3d printer or anything i can attach to it and have at least 4 axis possibly 5 image