Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Breakthroughs in the Realm of Technology
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 10 Jun 2010 1:51 AM Date Created
  • Views 629 views
  • Likes 0 likes
  • Comments 0 comments
  • player
  • consumer
  • phone
  • cell
  • unlock
  • electronics
  • mp3
Related
Recommended

Breakthroughs in the Realm of Technology

e14 Contributor
e14 Contributor
10 Jun 2010
Scientifically, the term ‘electronics’ refer to that mode of technology directed towards channelizing the electrons through media to project an audio and visual manifestation. These are in the form of cell phones, iPhones, iPods, MP3 players and more. Nevertheless, you should learn about a few functions related to the electronic goods that will enable you to access the devices with convenience.
 
The Three Most important Breakthroughs in the realm of technology:
 
Learning to unlock Cell Phones
 
The cell phone uses a certain technique to unlock cell phones. You need the phone number of the phone that is used, the IMEI number, the model number and the network which has certified the phone’ locking system.
 
The system to unlock cell phones follows a few simple rules. You may use the simple device by the cell phone company or see help from the operator to unlock. You may also send your phone directly to the company for unlocking it, but remember to reimburse the service charges. The best way to avert the hassles is to send the IMEI number to the company in exchange for IMEI code, to unlock.
 
What is Garmin GPS?
 
GPS or the Global Positioning system is used to track the location of a person on Earth. The GPS uses the integrated system of receivers and satellites so as to find the precise positioning. It is very accurate since it uses the parallel system of the multi-channel.
 
Thanks to Garmin, since it uses about 12 parallel channels for receiving the signal even through the very dense forest or through the skyscrapers that you might think obstruct the signal flow. One thumbs up for Garmin GPS receiver is that it operates precisely within 15 meters, which is on the average. Nevertheless, with technology unleashing surprises at every turn of the road, the Garmin GPS receiver is now configured with the WAAS system, that is Wide Area Augmentation System to operate within 3 or 4 meters.
 
The Fun of MP3 Player
 
MP3 player is the small device that can be carried in pockets. It uses the precise technology of MP3 format so that you can transfer the MP3 files to the format. You can do the copy from various sources like CDs, radio, websites and personalize the list you want to. The CD players, the mini or hard drive players and Flash memory players are the types of MP3 players, which are useful.