Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Building the Asuro Robot (Week 1) - Switches and resistors
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 26 Oct 2014 6:21 PM Date Created
  • Views 485 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Building the Asuro Robot (Week 1) - Switches and resistors

e14 Contributor
e14 Contributor
26 Oct 2014

Date: 06/10/2015

Week 1

 

Farnell, Leeds

Laboratory Report

Objectives

 

The objectives for this week was to start constructing the Asuro Robot. This was to be achieved by soldering the six switches to the front of the front of the robot with the corresponding resistors.

 

Equipment Required

 

Solder Iron

Multimeter

Solder

Wire cutters

Asuro Robot kit

PDF about the robot

 

Execution



Firstly the kit had to be opened to obtain the CD ROM containing the PDF file showing the circuit diagram and the resistor values. The kit was also examined for any missing parts or obvious defects to the circuit board, which luckily there was nothing outstanding. Soon after, the resistors got sorted into groups with equal value, to help determine that the PDF also contained the sequences for the resistors and the number that corresponds to their place on Asuro.


image

Above is the circuit diagram of the Asuro Robot.

 

 

image

Above shows the series of resistors.

 

Once the resistors have been separated into their own piles dictated by their Ohms, , the switches (K) got soldered on and so did the resistors at places R24 to R30. The voltage drops were then tested through R24 using a multimeter, the results were

 

ResistorVoltage Drop (V)
R253.4
R26 and R324
R27

4.5

R284.7
R294.88
R304.9

   

The voltage drops were within +/-20% of the recommended allowance.

 

These drops are required for later on after the build when the programming begins as when one or more switches have been activated the robot can react to any changes such as rotating or reversing.

 

 

image

Above is the finished goal with the switches and resistors soldered on to the switch board.