Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs C&C: The Wimpy Robot Bumper Class
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: alanmcdonley
  • Date Created: 25 Jun 2016 2:05 AM Date Created
  • Views 498 views
  • Likes 0 likes
  • Comments 0 comments
  • python-control-c
  • python-callbacks
  • python-threads
  • bumpers
  • python-class
Related
Recommended

C&C: The Wimpy Robot Bumper Class

alanmcdonley
alanmcdonley
25 Jun 2016

Here is the Bumper Class with polling thread to read the bumpers asynchronously from the consumer (test main() in the same file) and my control-c handler that can call a class object's cancel function to kill the thread and clean up: (I have the feeling I don't need the global statements.)

 

[code]

#

# myPyLib.py   SUPPLIMENTAL PYTHON FUNCTIONS

#

# v0.1 19June2016

 

import time

import sys

import signal

 

# ######### CNTL-C #####

# Callback and setup to catch control-C and quit program

 

_funcToRun=None

 

def signal_handler(signal, frame):

  print '\n** Control-C Detected'

  if (_funcToRun != None):

     _funcToRun()

  sys.exit(0)

 

# Setup the callback to catch control-C

def set_cntl_c_handler(toRun):

  global _funcToRun

  _funcToRun = toRun

  signal.signal(signal.SIGINT, signal_handler)

[/code]

[code]

#!/usr/bin/python

#

# bumbersClass.py   BUMPERS SENSOR CLASS

#

 

 

import PDALib

import myPDALib

import myPyLib

import time

import sys

import threading

 

 

 

 

class Bumpers():

 

 

  # CLASS VARS (Avail to all instances)

  # Access as Bumpers.class_var_name

 

 

  pollThreadHandle=None   # the SINGLE read sensor thread for the Bumpers class  

  tSleep=0.033            # time for read_sensor thread to sleep after each read op

 

  # Bumpers are on the Pi Droid Alpha MCP23S17 DIO expander

  # Wired to use internal pull-up power of the MCP23S17

  # Bumper value is negative logic - 0 means bumper activated, normal 1

 

 

  LeftBumperDIO=18

  RightBumperDIO=17

  RearBumperDIO=16

 

 

  # Allowable Bumpers.state values

  NONE     = 0

  # Single bumpers

  LEFT     = 1  

  RIGHT    = 2

  REAR     = 4

  # Combinations

  FRONT    = 3

  LEFTREAR = 5

  RIGHTREAR= 6

  ALL      = 7

  # Not possible

  UNKNOWN  = 8

 

  # THE STATE OF EACH BUMPER and the combined BUMPERS state

  # (class vars because there are only one physical bumper)

  # note: can get rid of left(), right(), rear() methods by using these vars direct

  leftState= UNKNOWN

  rightState=UNKNOWN

  rearState= UNKNOWN

  state=     UNKNOWN  #0,1=L,2=R,3=L+R(front),4=Rear,...

 

 

  # use to print Bumper.state var

  bumperStrings=["NONE", "LEFT", "RIGHT", "FRONT", "REAR",

               "LEFTREAR", "RIGHTREAR", "ALL", "UNKNOWN"]

 

  # end of class vars definition

 

 

  def __init__(self):

    # SINGLETON TEST

    if (Bumpers.pollThreadHandle!=None):

        print "Second Bumpers Class Object, not starting pollingThread"

        return None

 

    # Set Bumper DIO channels as input for now

    PDALib.pinMode(Bumpers.LeftBumperDIO, PDALib.INPUT)

    PDALib.pinMode(Bumpers.RightBumperDIO,PDALib.INPUT)

    PDALib.pinMode(Bumpers.RearBumperDIO, PDALib.INPUT)

 

 

    # Set internal pull-ups on bumper channels

    PDALib.setDioBit( PDALib.DIO_GPPU, 8 )  # set LeftBumper  pin 16 pull-up

    PDALib.setDioBit( PDALib.DIO_GPPU, 9 )  # set RightBumper pin 17 pull-up

    PDALib.setDioBit( PDALib.DIO_GPPU, 10 ) # set RearBumper  pin 18 pull-up

    # threading target must be an instance

    Bumpers.pollThreadHandle = threading.Thread( target=self.pollBumpers,

                                               args=(Bumpers.tSleep,))

    Bumpers.pollThreadHandle.start()

  #end init()

 

 

  # BUMPER THREAD WORKER METHOD TO READ BUMPERS

  def pollBumpers(self,tSleep=0.01):    

    print "pollBumpers started with %f" % tSleep

    t = threading.currentThread()   # get handle to self (pollingBumpers thread)

    while getattr(t, "dorun", True):  # check the dorun thread attribute

      self.read()

      time.sleep(tSleep)

    print("dorun went false. Stopping pollBumpers thread")

 

 

   

  def read(self):  #READ THE BUMPERS - can be used as poll or directly

      Bumpers.leftState= Bumpers.LEFT - Bumpers.LEFT * \

     PDALib.digitalRead(Bumpers.LeftBumperDIO)

      Bumpers.rightState= Bumpers.RIGHT - Bumpers.RIGHT * \

       PDALib.digitalRead(Bumpers.RightBumperDIO)

      Bumpers.rearState=  Bumpers.REAR - Bumpers.REAR * \

    PDALib.digitalRead(Bumpers.RearBumperDIO)

      Bumpers.state = Bumpers.leftState + Bumpers.rightState + Bumpers.rearState

      return Bumpers.state

 

 

  def status(self):

    return Bumpers.state

 

 

  def left(self):

    return Bumpers.leftState

 

 

  def right(self):

    return Bumpers.rightState

 

 

  def rear(self):

    return Bumpers.rearState

  

  def toString(self,bumperState=UNKNOWN): 

    if (bumperState==Bumpers.UNKNOWN):

       bumperState= Bumpers.state

    return Bumpers.bumperStrings[bumperState]

 

 

  def cancel(self):

     print "bumpers.cancel() called"

     self.pollThreadHandle.dorun = False

     myPDALib.PiExit()

 

 

 

 

# ##### BUMPER CLASS TEST METHOD ######

# creates two instances, only the first should start the read() thread

# the first time through the main() while loop, the sensors may not have been read yet

#     so bumpers.status() and each bumper may have a value of 8/UNKNOWN

def main():

  # note: lowercase bumpers is object, uppercase Bumpers is class (everywhere in code)

  bumpers=Bumpers()  #create an instance which starts the read bumpers thread

  bumpersNoThreadStart=Bumpers()  # Test a second instance of class

  myPyLib.set_cntl_c_handler(bumpers.cancel)  # Set CNTL-C handler

  while True:

      print "\n"

      print "bumpers.state: %d %s" % (bumpers.status(), bumpers.toString())

      print "left():%d  rear():%d  right():%d" % (

  bumpers.left(),

  bumpers.rear(),

  bumpers.right() )

      time.sleep(1)

  #end while

 

 

 

if __name__ == "__main__":

    main()

 

 

 

[/code]