Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Chaining AXI Streams together
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tcmichals
  • Date Created: 26 Aug 2020 4:05 AM Date Created
  • Views 1296 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Chaining AXI Streams together

tcmichals
tcmichals
26 Aug 2020

Background

 

In my last blog there was an example of a AXI Stream between the DMA IP and UART IP, here the module definition (from github)

 

module uart_axis #(    parameter CLKS_PER_BIT = 16 )

(

    /*

     */

    input  wire       axis_aclk,

    input  wire       axis_reset,

 

    /*

     * AXI input

     */

    input  wire [7:0]  s_axis_tdata,

    input  wire        s_axis_tvalid, 

    output wire        s_axis_tready,

 

    /** AXI output   */

    output wire [7:0]  m_axis_tdata,

    output wire        m_axis_tvalid,

    input  wire        m_axis_tready,

    output wire         m_axis_tlast,

 

    /*

     * UART: 1200000 bps, 8N1

     */

    input  wire       uart_rxd,

    output wire       uart_txd

      

);

 

DMA IP connects to m_axis_* and s_axis, and uses tready as flow control.  It is possible to chain several of these modules together m_axis to s_axis.  Instead of having one big file, connect each one back to back.

Serial protocol

The microblaze handles a lot of the encoding/decoding/CRC of the packet, see basicProtocol::onRecv and basicProtocol::sendPacket protocol.h in github.  So, I have been working breaking up the code into 3 AXI streams

  1. CRC AXI Stream module to do append a CRC at the end of the data (this replace computing the CRC in basicProtocol::sendPacket.
    1. There is a good Verilog code generator to create the proper code to calculate a CRC in parallel for a user defined polynomial.  For code example see github here is a simple test-bench
    2. Wrapped the CRC code to reset the CRC back to 0xFFFF and add it to the end of the stream when TLAST is asserted.  See github)
  2. AXI Stream to perform the packet formatting, the last part of the function basicProtocol::sendPacket.
    1. The first byte of the packet must be SOP (0x7E)
    2. If the SOP, EOP or ESC is in data stream replace with ESC and add the data xor'ed with 0x20.
  3. AXI Stream for TX serial.

 

I have been working on a single test bench using verilator to use the C++ code to generate ping  (without CRC and ESC processing) send it to the Verilog stream for calculating the CRC and ESC formatting then pipe the bytes back to C++ for decoding.  (That will be the next blog)  Here is a start of the test bench.

  • Makefile
  • axis_tx_protocol_tb.cpp
  • axis_tx_protocol_tb.v