Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Control smart RGBW LEDs from your Tibbo Project System
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dmitry_slepov
  • Date Created: 26 Sep 2016 1:12 PM Date Created
  • Views 1126 views
  • Likes 0 likes
  • Comments 4 comments
  • tps
  • leds
  • tibbo
Related
Recommended

Control smart RGBW LEDs from your Tibbo Project System

dmitry_slepov
dmitry_slepov
26 Sep 2016

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

You will need:

  • TPP2, TPP2(G2), TPP3, or TPP3(G2) board
  • One Tibbit #57
  • One Tibbit #20
  • Optionally, one Tibbit #00-3 (if you are going to power your smart LEDs from your TPS system)
  • Several SK6812RGBW LEDs (or a board, or an LED strip containing these LEDs).
  • Optionally, one Tibbit #10 (12V->5V regulator)
  • Optionally, one Tibbit #18 (power jack)

The last two Tibbits are necessary if you are going to power your rig from a 12V power adaptor. Alternatively you can supply regulated +5V power directly to the TPP.

Tibbit #57 is based on the ICE5LP2K-SWG36ITR50 FPGA from Lattice Semiconductor. This FPGA is suitable for a large number of projects. One such project is the smart LED controller.

In the smart LED configuration, Tibbit #57 can control a string of daisy-chained SK6812RGBW LEDs. SK6812RGBW devices carry a small IC driving four onboard light emitters with red, green, blue, and white colors. Each of the color sources can be set to one of the 256 levels of brightness, meaning that four bytes of data are needed per LED.

Smart LEDs are controlled via a special 1-wire protocol. Each LED has a DIN (data in) and DOUT (data out) pins. The DIN pin of the first LED in the chain is connected to the IO1 line of the FPGA Tibbit. The DOUT of the first LED is connected to the DIN of the second LED, the DOUT of the second LED — to the DIN of the third LED, and so on.

image

Depending on the number of LEDs you are connecting, you may be able to power them from your TPS, or you may need to use an external +5V power supply. R, G, and B emitters of each LED consume up to 9mA each, the white emitter consumes up to 18 mA. Count the available current and choose the right power source!

Before you run the application, set the actual number of LEDs you have connected in the "Const NUM_LEDS=" line.

The test application has three modes — PATTERN_1, PATTERN_2, PATTERN_3. Select the mode in the "Dim pattern_mode as pattern_modes=" line.

PATTERN_1: All LEDs set to the same color, the color will gradually change from R to G, from G to B, and from B to R.

PATTERN_2: A moving pattern of RGB colors.

PATTERN_3: White LEDs all set to the same brightness, and the brightness gradually changes between minimum and maximum.

The longer your LED chain is, the slower the "animation" runs. If you have a small number of LEDs connected (10-20), then you may discover that everything changes too fast. In that case, increase the delay specified by the "Const LED_OUTPUT_DELAY=" line.

 

Originally published at: tibbo.com

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago in reply to Jan Cumps +1
    I must have missed Peter's post. Very impressive design and ease of use. DAB
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to DAB +1
    They are a good design, makes me think of Lego for sure and there software / firmware is pretty much complete, as of the time of posting this, it is very easy to get Node-red, MQTT, SQLite3 etc up and…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to DAB

    They are a good design, makes me think of Lego for sure and there software / firmware is pretty much complete, as of the time of posting this, it is very easy to get Node-red, MQTT, SQLite3 etc up and running and I have created a few nodes for Node-Red to directly talk to the modules I have. A fun project indeed. And a very good experiance with their technical support folks who were awesome in addressing concerns and providing resolutions to my review efforts.

    Most impressed image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago in reply to Jan Cumps

    I must have missed Peter's post.

     

    Very impressive design and ease of use.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    Tibbo is industrial/domotica grade, DAB.

    Our very own Robert Peter Oakes has made a nice overview:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    How does this product differ from Adafruit products?

     

    DAB