Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Correctly Installing Brian 2 Simulator for windows 7 64-bit
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mohanedessam
  • Date Created: 14 Nov 2015 10:10 AM Date Created
  • Views 1396 views
  • Likes 0 likes
  • Comments 0 comments
  • python
  • brian2_simulator
  • brian2
  • install
  • anaconda
  • spiking_neural_networks
Related
Recommended

Correctly Installing Brian 2 Simulator for windows 7 64-bit

mohanedessam
mohanedessam
14 Nov 2015

I did this blog post especially because I had some hard time installing the Brian2 simulator, even though I followed all the instructions in the official documentation Link

 

I tried many time until l found a working method, which is using an older version of "matplot" library to avoid upgrading the numpy package, although this method provides Brian testing without any errors, I am not sure what are the implications of that, as I am not experienced in Brian2, but anyway I hope it may benefit anyone struggling too:

 

1- I downloaded the Anaconda python 2.7 version for 64-bit windows from this link (the version I used is shown in the image)

image

2- I installed Anaconda from its executable file following all the default settings

 

3- I installed the Brian2 team channel using the command :

conda config --add channels brian-team

image

4- I installed Brian 2 package:

conda install brian2

image

5- I installed other required packages:

conda install nose ipython ipython-notebook

image

6- I installed an older version of matplot library (so that I won't need to update numpy):

pip install -i https://pypi.anaconda.org/pypi/simple matplotlib

image

7- As this is the sequence in the original documentation, I should install the Microsoft Visual C++ Compiler for Python 2.7 from this link (but I actually had it installed before I setup Anaconda).

 

8- I typed "python" to get to the python terminal and performed the Brian2 testing:

import brian2
brian2.test()