Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Crawling Worm Robot
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 11 Dec 2020 5:46 PM Date Created
  • Views 3553 views
  • Likes 11 likes
  • Comments 9 comments
  • worm robot
  • crawling robot
Related
Recommended

Crawling Worm Robot

dubbie
dubbie
11 Dec 2020

I have seen these crawling worm robot kits around for some time and always thought they looked interesting, so while I was buying other people Christmas presents, I bought one for myself as well.

 

image

 

It has some neat design features to make it simpler to construction and low cost. The battery compartment comes with a built-in switch. Not a good picture below  but you can just about see the lever that you turn to make a contact with the other battery terminal.

 

image

 

It probably took about an hour to put together and it does have some very small screws and some fiddly assembly sequences. Additionally the instructions were in Chinese but by carefully viewing the diagrams on the leaflet and overcoming my fat fingers and less that perfect eyesight I managed to put it together.

 

image

 

A fascinating motion. It truly zips along at some speed.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Technically, it is not a robot as it does not have any sensors or even a controller, but I think it would be relatively easy to add an Arduino of some description, plus a sensor, and then it will be able to interact with it's environment. I wonder if I can connect two or more together to make a much longer worm?

 

Dubbie

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 5 years ago +5
    Is this 'bait' for your cat detector ? genebren this type of action may drive your whistle bellows for your Mr Machine
  • DAB
    DAB over 5 years ago +4
    Nice build. It would cause my dog to attack it immediately. She likes to chase anything that moves. DAB
  • ntewinkel
    ntewinkel over 5 years ago +3
    Aahaha that's awesome! Is the worm action used to propel it forward, or is all of that just in the drive wheels? -Nico
Parents
  • ntewinkel
    ntewinkel over 5 years ago

    Aahaha that's awesome!

     

    Is the worm action used to propel it forward, or is all of that just in the drive wheels?

     

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 5 years ago in reply to ntewinkel

    Nico,

     

    Yes, it is the worm action that propels it forwards. The white wheels are unpowered and just roll. It is something to do with the momentum and although not easily visible, there are two elastic bands which I thought couldn't be doing much, but it works much better when they are installed. I might have a go at trying to think about how it works - although I'm not sure I have the brain power to do that any more. It must be fairly simple physics and conservation of energy (momentum? ). I might have to read some physics.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 5 years ago in reply to ntewinkel

    Nico,

     

    Yes, it is the worm action that propels it forwards. The white wheels are unpowered and just roll. It is something to do with the momentum and although not easily visible, there are two elastic bands which I thought couldn't be doing much, but it works much better when they are installed. I might have a go at trying to think about how it works - although I'm not sure I have the brain power to do that any more. It must be fairly simple physics and conservation of energy (momentum? ). I might have to read some physics.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down