Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Create a Programmable Instrument with SCPI - Part 4: Error Handling by Default
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Sep 2016 9:42 AM Date Created
  • Views 2310 views
  • Likes 2 likes
  • Comments 1 comment
  • smart_instrument
  • gpib
  • usb
  • labview
  • scpi
Related
Recommended

Create a Programmable Instrument with SCPI - Part 4: Error Handling by Default

Jan Cumps
Jan Cumps
24 Sep 2016
For a hardware evaluation project I'm working on, I want to create a device that can be controlled via LabView.
LabView can talk to instruments using serial out of the box, and it knows how to talk Standard Commands for Programmable Instruments (SCPI).

 

image

 

In this blog I'm checking the excellent error handling of the SCPI library.

 

 

Error Handling Works by Default

The SCPI parser library that I use has out-of-box support for standard behaviour. One of the supported features is error handling.

If you send a bogus SCPI command or make a syntax error, this is registered by the library.

The error description is pushed on an error stack. The parser returns to its normal work.

As an instrument firmware designer, you can also push custom error situations to the error stack.

A possible use case is for a PWM generator where the user requests a frequency higher than the maximum.

 

You can check if errors occurred by sending the SCPI command:

SYST:ERR:COUN?

 

If errors happened, you get a number back. That's the count of errors on the stack.

e.g.:

5

 

Each error can be retrieved by firing:

SYST:ERR?

 

A possible return value (one of the default error messages from our parser lib):

-113,"Undefined header"

 

Each time you ask an error message, the error is popped off the stack and the error count decreases.

When you've retrieved the last message, you get the following reply when shooting a  SYST:ERR:COUN? :

0

 

If you check for an error message when the error stack is empty, (SYST:ERR?), you get:

0,"No error"

 

You get all this functionality by default and you can tap into it in your own firmware. Another worry taken out of your hands by this library.

Other standard constructs that are either fully supported, or give you an easy implementation hook are:

 

    { .pattern = "*CLS", .callback = SCPI_CoreCls,},
    { .pattern = "*ESE", .callback = SCPI_CoreEse,},
    { .pattern = "*ESE?", .callback = SCPI_CoreEseQ,},
    { .pattern = "*ESR?", .callback = SCPI_CoreEsrQ,},
    { .pattern = "*IDN?", .callback = SCPI_CoreIdnQ,},
    { .pattern = "*OPC", .callback = SCPI_CoreOpc,},
    { .pattern = "*OPC?", .callback = SCPI_CoreOpcQ,},
    { .pattern = "*RST", .callback = SCPI_CoreRst,},
    { .pattern = "*SRE", .callback = SCPI_CoreSre,},
    { .pattern = "*SRE?", .callback = SCPI_CoreSreQ,},
    { .pattern = "*STB?", .callback = SCPI_CoreStbQ,},
    { .pattern = "*TST?", .callback = SCPI_CoreTstQ,},
    { .pattern = "*WAI", .callback = SCPI_CoreWai,},

 

 

Test with PuTTY

 

When you want to test special conditions, it's often easier to use a terminal program than LabVIEW. You can just type away, and the results arrive in the parser lib immediately.

 

When I try to simulate a real test environment, I mock it with LabVIEW. But when I try to exercise a particular part of the library, or want to see how my firmware reacts on each single character (valid or invalid), plain old PuTTY is easier.

 

PuTTY is also easy to learn the SCPI parser lib. Set a breakpoint in the SCPI_Input() function and type *IDN?<enter> in PuTTY. Your code breaks at each character you type. You can step trough the logic that builds up the command string. You'll also see how the library recognises when it received a full command.

You can then step trough the execution of the code that implements that command.

If you do that a few times, you'll get a deep understanding of the library. It 'll help you to extend it in the right way.

 

Related Blog

Create a Programmable Instrument with SCPI - Part 1: Parser Library
Create a Programmable Instrument with SCPI - Part 2: Serial over USB
Create a Programmable Instrument with SCPI - Part 3: First Conversation *IDN?
Create a Programmable Instrument with SCPI - Part 4: Error Handling by Default
Create a Programmable Instrument with SCPI - Part 5: First Hardware Commands
Create a Programmable Instrument with SCPI - Part 6: LabVIEW Integration
Create a Programmable Instrument with SCPI - Part 7: Talk to Hardware Registers
  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +1
    Nice update Jan. I agree, it is always best to start with the defaults until you get a full appreciation for which errors you need to specifically deal with. DAB
Parents
  • DAB
    DAB over 9 years ago

    Nice update Jan.

     

    I agree, it is always best to start with the defaults until you get a full appreciation for which errors you need to specifically deal with.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Nice update Jan.

     

    I agree, it is always best to start with the defaults until you get a full appreciation for which errors you need to specifically deal with.

     

    DAB