Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DC Motor Mobile Robot : With Nano Controller
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 16 Jun 2019 5:50 PM Date Created
  • Views 996 views
  • Likes 4 likes
  • Comments 3 comments
  • nano
  • 3D Printing
  • mobile robot
  • robotics projects
  • arduino
Related
Recommended

DC Motor Mobile Robot : With Nano Controller

dubbie
dubbie
16 Jun 2019

I took the Nano controller that I used with the small train from my SuperRobot and just reconnected it to the battery and DC motors on my DCMotorMobot. This is all connected outside the 3D printed shell so is just dragged or pushed along but I wanted to make sure that the motor driver H bridge PCB that I was using would work with these motors, as it didn't work very well with my SuperRobot. As you can see from the video below, it all worked fine.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I have purchased some Arduino Nano's without the connector pins installed which arrived very quickly so that it will fit into the base compartment of my robot chassis, along with a dual DC motor driver PCB. Unfortunately, at present, the Nano will not upload a programme. I'm not sure why as I have a driver for the CH340 installed and I have selected Nano so it should work. I'll have another look at this sometime tomorrow or later.

 

Dubbie

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +2
    Dubbie, Glad to see that the motor driver is working well with your motors! That is always a good thing. Keep up the good work, as this is already looking to be quite a successful robot project. Gene
  • dubbie
    dubbie over 7 years ago in reply to genebren +1
    Gene, It has been a fun build. It is the first mobile robot that is fully 3D printed that I have created. I made it from the 3D printing inwards so I still have to fit the electronics inside - hopefully…
  • genebren
    genebren over 7 years ago in reply to dubbie +1
    Dubbie, Building and printing is an iterative process. The more that you build, the better your skill set becomes. In printing, I find, as soon as I complete a print I discover several things that I would…
Parents
  • genebren
    genebren over 7 years ago

    Dubbie,

     

    Glad to see that the motor driver is working well with your motors!  That is always a good thing.  Keep up the good work, as this is already looking to be quite a successful robot project.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Dubbie,

     

    Glad to see that the motor driver is working well with your motors!  That is always a good thing.  Keep up the good work, as this is already looking to be quite a successful robot project.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dubbie
    dubbie over 7 years ago in reply to genebren

    Gene,

     

    It has been a fun build. It is the first mobile robot that is fully 3D printed that I have created. I made it from the 3D printing inwards so I still have to fit the electronics inside - hopefully I'll be able to do this. I'm already thinking of my next build where I will start with the electronics and work outwards to the 3D printed shell.

     

    Then much further into the future I want to design my own PCBs. I have done this before using a package called Proteus but I no longer have this software so I am thinking of using Eagle instead. I wasn't that good at it and tended to stick to single sided PCBs but it avoided all the messy wiring that I currently end up with.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to dubbie

    Dubbie,

     

    Building and printing is an iterative process.  The more that you build, the better your skill set becomes.  In printing, I find, as soon as I complete a print I discover several things that I would do differently and I am tempted to redesign the part and start over.

     

    The PCB design process is a lot of fun for me.  I see it almost like solving a puzzle or riddle, you just keep moving things around until you find the solution.  I have been using Eagle for more than 15 years.  I have tried a few of the other free or vendor supplied tool sets, but I always come back to Eagle.  Double sided PCBs are really not too much more complex than single sided, plus you get greater density designs having two sides to mount components and run traces.

     

    Keep building!

    Gene