Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Dexi Numeral System
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fahrenheit_98
  • Date Created: 27 May 2014 1:33 PM Date Created
  • Views 1220 views
  • Likes 0 likes
  • Comments 4 comments
  • Math
  • numeral_system
  • dexi
Related
Recommended

Dexi Numeral System

fahrenheit_98
fahrenheit_98
27 May 2014

It is well known that we use the Decimal Numeral System just because we have ten fingers.

 

It is also well known that the numeral systems with base two and multiples of two make the calculations much easier, compared to the use of the decimal system.

 

Unfortunately we do not have an easy to use symbolgy for the most powerful numeral systems:  we use part of the decimal symbols (binary and octal systems) or mixed decimal and alphabetic symbols (exadecimal system).

 

I propose the "Dexi Numeral System", a new exadecimal symbology where the symbols have a binary structure.

 

The system is very easy to learn and the calculations are  made easier by the power of the exadecimal and binary systems.

 

Some operations are also "easy to see".  Try, for example, to do a multiplication by two:  you just need to shift to left all the segments of the original number.

 

The proposed system is, of course, just an amusing exercise but, maybe, in one or two millenia we will use something similar.

  • Sign in to reply
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    What makes you think that "numeral systems with base two and multiples of two make the calculations much easier"  -for computers yes, for people ????

     

    Your zero symbol - won't do for me, it's already in use so we might end up with "if a == -e" which might mean "if a == -13" or "if a == 013".

     

    Actually I'm happy with "if a == 0xd" - but only because I'm used to it.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 12 years ago

    What makes you think that "numeral systems with base two and multiples of two make the calculations much easier"  -for computers yes, for people ????

     

    Your zero symbol - won't do for me, it's already in use so we might end up with "if a == -e" which might mean "if a == -13" or "if a == 013".

     

    Actually I'm happy with "if a == 0xd" - but only because I'm used to it.

     

    MK