Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DIY CRO TV
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: yesha98
  • Date Created: 20 Feb 2021 4:53 PM Date Created
  • Views 2648 views
  • Likes 8 likes
  • Comments 4 comments
Related
Recommended

DIY CRO TV

yesha98
yesha98
20 Feb 2021

I've always been interested in Cathode ray tubes, but the one that I got to play with is only the CRT inside an old TV.

One of the many ways in which an old TV can be reused is by converting it into an oscilloscope.

 

First, I hacked into the TV to see if something interesting could be made out of it.

image

The above image shows the electron gun which is used to fire the electron towards the fluorescent coated screen and the electro-magnets which are used to guide the electron beam in the right path.

Making some changes to the horizontal deflection coil or the vertical deflection coil, we'll be able to convert it into a basic scope, however, we need to add some impedance matching circuits since the passive element we're handling here has a notable inductance value. 

 

image

Source: https://www.schoolphysics.co.uk/age14-16/Electricity%20and%20magnetism/Electrostatics/text/Cathode_ray_oscilloscope/imag…

 

We'll be able to see the waveform of an input voltage given to the Y-axis deflection plate, that'll be the single channel input.

 

Here are some easy steps to follow:

VDC: Vertical Deflection Coil

HDC: Horizontal Deflection Coil

Firstly, disconnect the VDC and HDC from the main circuit board. Now connect the HDC where the VDC was initially connected in the circuit board. Attach two long wires to the VDC which will be the input to the oscilloscope. Now in case you need more precision, adjust the refresh rate by tuning the presets present in the circuit board.

 

Upon completing the above steps, once the TV is switched on,

image

This straight line indicates that the above-performed steps are correct.

Testing the scope with sample input:

image

With a basic transistor switch input, we can see the ON-OFF transients clearly!

image

Square wave input

image

Sine wave generated using PWM from Arduino

Finally, connecting one channel of an audio amplifier to the CRO TV to check the working!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Thanks for reading!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +2
    Nice mod, just be aware that standing or sitting in front of a crt at close distance can be harmful. You can get a small amount of X-ray exposure through the front. DAB
  • dubbie
    dubbie over 5 years ago +1
    A good project. I always wanted to make my own oscilloscope but just didn't have enough knowledge. I'm not sure I would have made one from a CRO TV though - far too many volts flying around. Now I have…
  • yesha98
    yesha98 over 5 years ago in reply to dubbie +1
    Neither did I, that's why tried out some cool stuff, also I was very much careful with the high-voltage transformer. I'm satisfied with the end-results indeed! Happy to know that now you own a DSO! I wish…
Parents
  • dubbie
    dubbie over 5 years ago

    A good project. I always wanted to make my own oscilloscope but just didn't have enough knowledge. I'm not sure I would have made one from a CRO TV though - far too many volts flying around. Now I have a digital storage oscilloscope - which I am very happy with.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 5 years ago

    A good project. I always wanted to make my own oscilloscope but just didn't have enough knowledge. I'm not sure I would have made one from a CRO TV though - far too many volts flying around. Now I have a digital storage oscilloscope - which I am very happy with.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • yesha98
    yesha98 over 5 years ago in reply to dubbie

    Neither did I, that's why tried out some cool stuff, also I was very much careful with the high-voltage transformer.

    I'm satisfied with the end-results indeed!

    Happy to know that now you own a DSO!

    I wish I would too, soon!