Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DIY Soldering Station Part 3
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: adsicks
  • Date Created: 16 Mar 2017 3:53 PM Date Created
  • Views 2541 views
  • Likes 4 likes
  • Comments 15 comments
  • diy rework station
  • openscad
  • carpentry
Related
Recommended

DIY Soldering Station Part 3

adsicks
adsicks
16 Mar 2017

I made the clamp to hold my extra pair of hands in place yesterday. It took about an hour.

 

I started out measuring the base of my hands and making a 3D model in OpenScad.

 

image

To start my cuts I set my blade to take out approximately half of the height of the base of the hands. I put a mark on a scrap board and used it to set my saw.

image

Then a marked two scraps the same width as one of the legs...

image

And cross cut them at the set depth (mindful of my thumb. I didn't want to chop it off today).

image

 

Then I checked my depth against the base of my extra hands.

image

I made adjustments to my saw depth and cut it until I got it flush. Next, I went back to my model and looked at the cut lay out.

image

 

 

 

And marked my wood.

 

image

 

I did the cross cut first. I used a long piece of wood because I like my thumbs.

 

image

 

I went a little past the line to make sure my channels were deep enough. It is alright if they aren't as deep towards the line as I am about to cut the channel along the grain of the wood.

 

To mark the channel for the back of the base I line the back of my extra hands with the line, put a mark and marked it with a speed square.

 

image

image

 

Then I cut the channel to my marks. It is important to have a square edge to work with for this step.

 

image

 

I used one of the scraps from my first steps to check my depth with the extra hands.

 

image

I cut out the top part from the edge. I turned it around and marked the hole for the neck. I adjusted the saw to the table for a full cut and notched out the neck hole. I used the full board to make this safer.

 

image

 

I used a jig saw to finish out the notch. Then I cut my pieces out of the larger board and dry fitted it.

image

 

It also helps to put the hands in it at this point to see if it fits the way you want it.

 

When I was satisfied I started the gluing process. First I glued the risers on the base with Gorilla Glue...

image

 

And clamped.

image

 

I only left it clamped for 30 minutes since I was clamping the top part along the same axis. Then I glued the top part with more Gorilla Glue and clamped.

 

image

 

Then I drilled the hole to hold the front clamp on. The finished product holding the hands should look like this:

 

image

 

Here is the open scad code for the exploded view:

 

//Base

rotate([180,0,180])

translate([-4,0,0])

difference(){

cube([4,2,0.75]);

translate([1,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

   

translate([2.5,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

translate([-0.05,1,-0.00005]) cube([4.1,1.1,0.375]);

    translate([2,0.5,0]) cylinder(r=0.1875);

    

}

 

 

// Front clamp

 

 

translate([0,-1,0])

difference(){

    cube([4,1,0.75]);

    translate([1,-0.01,-0.00005])    cube([0.5,2.01,0.375]);

   

translate([2.5,-0.01,-0.00005])    cube([0.5,2.01,0.3751]);

    translate([2,0.5,0]) cylinder(r=0.1875);

  }

 

 

// Back clamp

 

translate([0,2,1])

difference(){

    cube([4,1,0.75]);

    translate([-0.05,-0.05,-0.0001]) cube([4.1,1.1,0.375]);

    translate([1.5,0,0]) cube([1,0.5,0.75]);

  

}

 

 

translate([0,1.25,.5]) cube([1,1,0.75]);

 

 

translate([3,1.25,.5]) cube([1,1,0.75]);

 

 

Thanks to my helper, Paul, who took the action shots....

  • Sign in to reply
  • COMPACT
    COMPACT over 9 years ago

    A FRIENDLY NOTE

    Be aware that your ESD mat is not a compliant ESD mat!

    I've just found out that the JAKEMY JM-Z16 is just a silicone mat with a very thin ESD coating that is very easily damaged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 9 years ago

    Are you related to or Norm Abram from the New Yankee Workshop?

    The clues are;

     

    1. Plenty of woodwork,

    2. The use of a Radial Arm Saw (Very rare in Australia),

    3. Your red flannelette shirt.

    4. Your carpentry set square being related to mine.

    image

     

     

    And do your Rabbets breed out of control?

    (Rabbet aka Rebate)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to DAB

    Nice build.

     

    How easy is it to learn SCAD?

     

    DAB

     

     

    Not hard. It is not point and click. Take a look at these tutorials

    <http://www.openscad.org/documentation.html> and play around with the

    code I have posted is your best bet. When I start placing all of these

    part together I will use some variables and modules to help out and

    clean it up, so stay tuned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adsicks
    adsicks over 9 years ago in reply to DAB

    Thank you. I am glad you like it.  OpenScad is not super hard, but it is not point and click. You have to write some code. However, the code is fairly easy to learn. Take a look at these tutorials to start out and play around with the code I posted. As I start to put all of the parts together I will post the cleaned up code with variables and modules to help out with the viewing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Nice build.

     

    How easy is it to learn SCAD?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<