Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Do you know Nextion TFT HMI Display?
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 16 Oct 2015 7:19 AM Date Created
  • Views 2326 views
  • Likes 0 likes
  • Comments 4 comments
  • hmi
  • tft
  • nextion
  • display
Related
Recommended

Do you know Nextion TFT HMI Display?

e14 Contributor
e14 Contributor
16 Oct 2015

Itead Studio Itead Studiois an innovative high-tech company that specializes in selling electronics products, PCB, PCBA.They provides one-stop services from production, customization, retail and wholesale, technology support to after-sales services. So far, Itead Studio has more than 120 online agents in the world. Itead Studio has independent Research Department to rapidly develop new products to meet electronic enthusiasts and industrial needs. With years’ efforts on open-source hardware and intelligent hardware, they has been recognized by many leading brands such as Intel, Atmel, TI and has become co-developer of several Fortune 500 enterprises.

image

What is Nextion?

 

In 2014, with a strong market sensitivity, Itead Studio seize the initiative to develop a new TFT display called Nextion TFT Human Machine Interface(short for Nextion below). You might ask what is nextion?

Nextion is a Seamless Human Machine Interface (HMI) solution that provides a controllable and visualized interface between a human and a process, machine, application or appliance. Nextion is mainly applied to IoT or consumer electronics field. Nextion provides a complete, high-quality display features for developing advanced graphical embedded applications in a smaller RAM, lower frequency MCU and a lower cost even. Undoubtedly, it is the best solution to replace those traditional LCD and LED Nixie tube.

image

image

image

Previously, engineers have only two choices for designing GUI. Some engineers choose LCD module which requires to write a mass of of source codes, which is a time-consuming and complicated job, not to mention the result may be unpleasant; While other engineers had to pay a large sum of money to buy large size expensive industrial level HMI display in the market. In most cases, a small size HMI displays means lower costs and more choices. Thanks to Itead Studio team, with their Nextion now available in the market, these problems no more exist.

image

image

Nextion Competitive Edge

 

Why Nextion beats other displays in the market? See below comparison table:

Code RequiredSizePriceFunction
NextionNOCompleteHigh cost-effectiveHigh
Traditional LCD ModulelYESSmallLowSingle-function
Industrial HMINOLargeVery HighHigh

Nextion is characterized by

*Complete size displays(2.4",2.8",3.2",3.5",4.3",5.0",7.0") *One serial port communicate with MCU *Fully functional software-a WYSIWYG editor *Character string commands, reduce debugging difficulty *Objective-oriented controlling method, easily change component attribute properties. *Online Simulator Function *Great compatibility-Nextion can work with all MCU boards with TX, RX serial port, such as Arduino, MCU-51, Raspberry Pi, PC, etc.

 

How to use Nextion?

 

Nextion solution includes the hardware part - a series of TFT displays and the software part - Nextion editor, where you can design your interface. After the designing in the software, you can run the interface you designed in 2 ways. 1.Upload your interface to a USB-TTL board through connecting your PC, and the TX and RX connect to Nextion TFT display. 2. Copy your tft file to a SD card, then insert it to Nextion display to download it.

Nextion TFT displays use only ONEserial port to do communicating, which helps you get rid of the wiring trouble. Nextion editor has mass components to meet your design requirements, such as button, text, progress bar, slider, timer, variable, gauge,waveform, etc. Simply drag and drop these components to the editing window to automatically compile, no need to spend much time to program for these components any more. Also, you can online simulate your interfaces in Debug window. Now you can design your interface in just 5-10 minutes, Nextion Editor reduces your 99% development workloads! With the help of this WYSIWYG editor, GUI designing is just a piece of cake.

image

image

 

Specification(Nextion Touch Panel)


image


Size2.4"2.8"3.2"3.5"4.3"5.0"7.0"
Color65K(65536)65K(65536)65K(65536)65K(65536)65K(65536)65K(65536)65K(65536)
Layout size
(L*W*H,mm)
74.4*42.9 *5.885*49.8*5.895*47.6*5.8100.5*54.94*5.45120*74*6.2133.5*84*6.2181*108*9
Active Area
(L*W,mm)
42.72*60.2670.2*49.880.90*47.685.50*54.94105.50*67.20118.50*77.55164.9*100
Visual Area
(L*W,mm)
36.72*48.9657.6*43.269.60*×41.7673.44*48.9695.04*53.86108*64.8154.08*85.92
Resolution
(pixel)
320*240320*240400*240480*320480*272800*480800*480
Touch typeResistiveResistiveResistiveResistiveResistiveResistiveResistive
Touches>1 million>1 million>1 million>1 million>1 million>1 million>1 million
BacklightLEDLEDLEDLEDLEDLEDLED
Backlight lifetime
(Average, hours)
>30,000>30,000>30,000>30,000>30,000>30,000>30,000
Brightness(nit)180180180180230250250
Weight(g)25.829.542.548.293.8128268
Flash(MB)44416161616
RAM(byte)2048204820483584204820482048
Datasheetclickclickclickclickclickclickclick


Project Demonstration

 

Now you have a concept for Nextion. Let me show you projects to help you get start using the displays. I’m sure you will be astonished by these amazing Nextion TFT HMI displays.

 

Watch more projects by Nextion TFT HMI displays: https://www.youtube.com/channel/UCIiO6ag7O3vSFFGONQGySvg

Nextion TFT HMI display is the best choice I can find in the current market. Formerly when I was designing my own projects, I used the so-called LCD and wrote a lot of code, which really got me headache. I always wondered why there is no better choice. Now Nextion is it. You cannot miss it. Get your own brand-new Nextion now at http://www.itead.cc/display/nextion.html.

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    OK, nice teaser add, but what does it COST?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to DAB

    Tks! Can you see the last link: Buy Nextion Display For Raspberry Pi and Arduino DIY Development From China Supplies iTead.cc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to DAB

    Tks! Can you see the last link: Buy Nextion Display For Raspberry Pi and Arduino DIY Development From China Supplies iTead.cc