Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs ELEC2645 Project - Week 20
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 14 Mar 2016 12:08 AM Date Created
  • Views 849 views
  • Likes 1 like
  • Comments 4 comments
Related
Recommended

ELEC2645 Project - Week 20

e14 Contributor
e14 Contributor
14 Mar 2016

ELEC2645 - Embedded Systems Project - 'Sensor-matic!'

 

The aim of the project is to create an interface between a distance and a temperature sensor and an LCD screen.

 

Noise Cancellation In The SRF02 Sensor

 

Purpose:

 

  • The SRF02 Distance Sensor is subject to interference when taking readings.
  • The readings can fluctuate massively - even when the sensor is held in one position against a stationary solid object (i.e. a wall).
  • Typically, the fluctuates jumped up by 200+ cm.
  • This effect was observed at multiple distances suggesting the interference is random as opposed to systematic.

 

Method:

 

  • The problem can be tackled in a number of different approaches.
  • The easiest method is to simply calculate an average.
  • This method requires that 'X' amount of readings are taken every iteration and summed together.
  • The total sum is divided by the 'X'.
  • This reduces the significance of random errors (although doesn't eliminate them).

 

Code:

 

  • The initial total distance (int totalDistance) is set to equal zero.
  • The number of readings (previously 'X') was selected to be 10.
  • A 'For Loop' counts through 10 readings per iteration and each time.
  • The value of the distance at each stage is added to the totalDistance variable.
  • The final total is divided by 10 to give an output distance.

 

// Cancelling Out Sensor Noise Fluctuations

 

            int totalDistance = 0; // Create a Total Function

 

            for (int iteration = 0; iteration < 10; iteration++) { // Loop Through 10 Iterations

 

                    totalDistance = totalDistance + srf02.getDistanceCm();

                   

                lcd.refresh();

            }

 

Results:

 

  • The output is shown on the Nokia LCD screen.
  • The output is less susceptible to interference - the variations are much closer to the truth value.
  • A very high value would still cause an inaccurate reading - the code can be improved to solve this problem.

 

Improvements:

 

  • Cumulative/Rolling Average - Rather than 10 readings being taken and then the average found. A cumulative average continuously calculates the average based on the current ten numbers in an array/sample space. On the eleventh reading, the first one is neglected and a new average is found. The process repeats by discarding the 'firsts' element in the array and entering in the 'tenth' and recalculating.

 

  • Current Method inc. Rejection - The current method of determining the average can be implemented however to determine more accurate values, extra code could be implemented which rejects a distance which is above/below by 30% of the previous. In order to make sure the average is unaffected, the rejected distance would need to be replaced with another value - perhaps the distance of the previous reading.
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to mcb1 +1
    Thank you for the sound advice! I will work on that today and fingers crossed it should correct itself. Jack
Parents
  • jw0752
    jw0752 over 10 years ago

    Hi Jack,

    I like your project. I deleted a previous comment as I made the mistake of thinking your distance sensor was analog and when I learned other wise my advice for stabilizing the reading was no longer applicable.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 10 years ago

    Hi Jack,

    I like your project. I deleted a previous comment as I made the mistake of thinking your distance sensor was analog and when I learned other wise my advice for stabilizing the reading was no longer applicable.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to jw0752

    Thank you John, I should have probably specified more clearly.

     

    Jack