Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Energy Harvesting from RF of Mobile networks
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tdbr
  • Date Created: 25 Nov 2016 12:43 PM Date Created
  • Views 612 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Energy Harvesting from RF of Mobile networks

tdbr
tdbr
25 Nov 2016

Project proposal

 

Bilal Ahmad (MCA)

Innovator, Researcher.

yattoo.bilal@rediffmail.com

Cell no: +91-9419548626

Srinagar Kashmir

 

It self-mobile charging circuit

proposals

Radio Waves Converts to Electricity/Electricity Capture From Space (Energy Harvesting) With The Help Of EMI Of Mobile Phone Networks

 

Introduction:

Radio Waves Converts to Electricity/Electricity Capture is a concept of Power captures from space, this concept is used in modern world because the modern world is world of mobile technology.  Sir I worked on small circuit and made a device of electronics and some metal which generates electricity (Harvesting Energy) and it charges a smart phone without any charging device or without any power source, this circuit is mainly fabricated on a mobile circuitry which automatically charges the mobile while the mobile is in use of calling, massaging or using the internet and it charges the mobile without any hassle

Objectives:

The circuit gives us the big advantage over today’s world, it gives the full support of mobile technology and also it is used in various places like mobile tower, in mobile towers there is more Electromagnetic Force and it gives sufficient electricity in mobile towers. The circuit is also used in two ways communications like wireless apparatus, cordless phones, dish antennas etc. the concept of this device or methods used in this device never be created.

Analysis:

In today’s mobile age, our cell phones keep us connected to everyone 24×7. Without mobiles, we’ll all be back to the Stone Age. But irrespective of their class, they all run on a battery which goes down at the end of the day. The smarter your phone, the sooner it runs out of charge. I found every one need the mobile charge without hassle. And when I found this problem worldwide and I research on this problem and found there is network towers on mobile display and later I think there is some power transfer in the mobile phone while it works, and here I got problem for capturing this energy but it is very difficult to capture the electricity from space because various researches has been done but nobody captures. Finally one day I was working on this project and I observe some electronics captures/converts the mobile signals into the small electricity and later I capture more than 20 volts of dc current.

Technical Specification:

The circuit is made up of different semiconductors and some metal the circuit is not complicated it is simply fabricate on mobile phones are wireless apparatus and it is also used in mobile towers. The circuit generates more than 20 volt and 0.600µAW to 2.5 Amp. In a one circuit power which is sufficient for charging and more than one is used on mobile towers. The method I used is Electromagnetic Field of mobile network believe this is a very appropriate topic for electricity from artificial/ natural power which we until not generate.

The figure.1, which demonstrates an energy harvester receiving antenna of mobile phone/mobile network towers, in agreement with a characterization of the present invention. The invention will first be explained in a very necessary behaviour, and then a more detailed, non-limiting example will be described further here in below.

The energy harvester circuit a receiver (Receiving Antennas) capable of receiving electromagnetic field energy with the semiconductors radiate by electromagnetic interference, which may be generated by EFF of radio waves (“250to 2500 MHz ”) or of different radio waves frequencies by an electrical mobile networks (Mobile, Towers etc.). Receiver converts the electromagnetic field energy to an electrical current for powering for charging a battery or super capacitor).

As is well known in the art, EMF strength is the strength of an emitted electromagnetic field at a mobile phone antenna measured in units of volts with a field strength meter. The average field strength of EMI related with “250 MHz” is about 0.3V and ‘900 MHz + is about 5 volt plus.

A voltage amplification element (booster), such as but not limited to, it may be in circuit with the output booster for increasing the voltage associated with the electrical current coming from receiver (antennas and circuit). An electrical storage element (Battery or Super-Capacitor) may store at least some of the current previous to its being used to charge or power a device.