Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Environmental Monitoring with TPS, Azure, and PowerBI
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dmitry_slepov
  • Date Created: 18 Aug 2016 9:14 AM Date Created
  • Views 663 views
  • Likes 0 likes
  • Comments 0 comments
  • microsoft
  • azure
  • tps
  • tibbo
Related
Recommended

Environmental Monitoring with TPS, Azure, and PowerBI

dmitry_slepov
dmitry_slepov
18 Aug 2016

Сollect environmental data with Tibbo Project System devices, process it with Azure Stream Analytics and visualize using Power BI.

 

image

Configure and Assemble the TPS

  • Open LTPS Web Interface by simply entering its IP address in your browser, select the "Tibbits Layout" tab, and push the "Launch TPS Configurator..." button.

 

LTPS Web Interface
LTPS Web Interface

 

  • Setup Tibbits Layout as shown on the screenshot below and click File/Save

Note: TPS needs to be rebooted to take new Tibbits Layout into effect.

 

Proposed tibbits layout
Proposed Tibbits layout

 

  • Assemble TPS according to the Tibbits Layout

Attention: it's strongly recommended to shut down TPS before placing/removing Tibbits.

 

Assembled device with the top cover removed
Assembled device with the top cover removed

 

Step 1: First application

Node.js, Git and Python 2.7 are installed on each LTPS by default, but NPM is not.

  • For installing, connect it to your device with SSH and do the following:

 

# Setup package repositories
smart channel --add 150a type=rpm-md name="LTPS all" baseurl=http://tibbo.com/downloads/LTPS/packets/all/ -y
smart channel --add 150c type=rpm-md name="LTPS cortexa" baseurl=http://tibbo.com/downloads/LTPS/packets/cortexa8hf_neon/ -y
smart update
# Install NPM
smart install nodejs-npm -y

 

 

then:

# Create folder for application
cd /opt/node-apps/
mkdir environment
cd environment
# Install required modules
npm install @tibbo-tps/tibbit-28
npm install @tibbo-tps/tibbit-30
npm install @tibbo-tps/tibbit-35

/opt/node-apps/ folder is proposed to be used for your Node.JS apps.

 

  • In any IDE or even a text editor create azure-app-0.js file with your application:

 

var tibbit28 = require("@tibbo-tps/tibbit-28").init("S11");
var tibbit35 = require("@tibbo-tps/tibbit-35").init("S13");
var tibbit30 = require("@tibbo-tps/tibbit-30").init("S15");
setInterval(function(){
  var illuminationData = tibbit28.getData();
  var humidityData = tibbit30.getData();
  var pressureData = tibbit35.getData();
  var dateTime = new Date();
  console.log("Date/Time: "+dateTime);
  console.log("Illumination: "+illuminationData.illumination);
  console.log("Humidity: "+humidityData.humidity);
  console.log("Temperature: "+humidityData.temperature);
  console.log("Pressure: "+pressureData.pressure);
},1000);

 


  • Upload it to /environment folder and run:

$ node azure-app-0.js
Date/Time: Tue Jul 19 2016 13:50:54 GMT+0000 (UTC)
Illumination: 115
Humidity: 43.755340576171875
Temperature: 28.05670928955078
Pressure: 738.7398681640625

 

Step 2: Setting Up Microsoft Azure IoT Hub

Microsoft Azure IoT Hub is a service that allows bi-directional communications between your devices and a solution back end. To complete this part of the tutorial you'll need:

  • TPS device(s) prepared as shown on the Step 0
  • An active Azure account
  • A PC with installed Node.js

Create an IoT Hub

  • Sign in to the Azure Portal
  • Choose New > Internet of Things > Azure IoT Hub
  • Configure your IoT Hub, then click "Create"
Azure Portal: Creating an IoT Hub
Azure Portal: Creating an IoT Hub
  • Wait a few minutes until your IoT Hub has been created then select All Resources > [name of your IoT hub] and click "Keys" icon.
  • In the Shared access policies blade select the "iothubowner" item and then copy the value of "Connection string" field.
Azure Portal: Setting up your IoT Hub
Azure Portal: Setting up your IoT Hub

Step 3: Registering Device Identities

There are three ways to register device identities: with a script using Azure API, with GUI App (for Windows only) and with multiplatform CLI tool. The third way seems to be the most convenient one.Note: To use iothub-explorer you need Node.js version 4.x or later installed

 

  • On your PC run:

npm install -g iothub-explorer@latest

 

  • then:

$ iothub-explorer login <connection-string>
Session started, expires Thu Jul 21 2016 13:22:10 GMT+0400


 

where <connection-string> is an iothubowner connection string from Step 2.

  • To register a new device and get its connection string:

$ iothub-explorer create <device-name> --connection-string
Created device tps-centreville
...
connectionString: HostName=iot-tps.azure-devices.net;DeviceId=tps-centreville;SharedAccessKey=fSCVQIY..TOprSsDE=

 

 

Where <device-name> is e.g. "tps-centreville".

  • Make note of the connections string.

Step 4: Making devices IoT-enabled

  • Connect with SSH to the TPS, change folder to /environment and do:

npm install azure-iot-device
npm install azure-iot-device-amqp


  • Create azure-app-1.js file with the following app:

var clientFromConnectionString = require('azure-iot-device-amqp').clientFromConnectionString;
var Message = require('azure-iot-device').Message;
var connectionString = '<THE DEVICE CONNECTION STRING FROM STEP 3>';
var client = clientFromConnectionString(connectionString);
var tibbit28 = require("@tibbo-tps/tibbit-28").init("S11");
var tibbit35 = require("@tibbo-tps/tibbit-35").init("S13");
var tibbit30 = require("@tibbo-tps/tibbit-30").init("S15");
client.open(function(err){
if(err){
   console.log('Could not connect: ' + err);
}else{
   console.log('Client connected');
  setInterval(function(){
   var illuminationData = tibbit28.getData();
   var humidityData = tibbit30.getData();
   var pressureData = tibbit35.getData();
   var time = new Date().toISOString();
   var data = JSON.stringify({
       deviceId: 'tps-centreville',
       humidity: humidityData.humidity,
       temperature: humidityData.temperature,
       pressure: pressureData.pressure,
       illumination: illuminationData.illumination,
       time: time
  });
   var message = new Message(data);
  client.sendEvent(message, function (err) {
   if(err){
        console.log(err.toString());
   }else{
        console.log("Message sent: " + message.getData());
   }
  });
  },60000)
}
});

 

 

  • Upload it to /opt/node-apps/environment folder on the TPS and run:

$ node azure-app-1.js
Client connected
Message sent: {"deviceId":"tps-centreville","humidity":37.1016960144043,"temperature":31.370407104492188,"pressure":742.8632202148438,"illumination":136,"time":"2016-07-21T10:19:07.490Z"}
Message sent: {"deviceId":"tps-centreville","humidity":37.1016960144043,"temperature":31.370407104492188,"pressure":743.2034301757812,"illumination":137,"time":"2016-07-21T10:20:10.582Z"}
Message sent: {"deviceId":"tps-centreville","humidity":37.1016960144043,"temperature":31.380477905273438,"pressure":743.2034301757812,"illumination":138,"time":"2016-07-21T10:21:12.003Z"}


Event monitoring is the most remarkable and very useful feature for the purpose of debugging iothub-explorer. With iot-explorer, you can easily observe events sent by your devices to cloud and vice versa.

Note: this command requires providing iothubowner connection string even if you're already logged in.

  • On your PC do:

$ iothub-explorer <connection-string> monitor-events tps-centreville
Monitoring events from device tps-centreville
Event received:
{ deviceId: 'tps-centreville',
humidity: 37.1016960144043,
temperature: 31.380477905273438,
pressure: 743.2034301757812,
illumination: 138,
time: '2016-07-21T10:21:12.003Z' }

 

 

You can see every event as soon as it's sent to IoT hub.

Step 5: Configure Stream Analytics

Note: To complete this part of the tutorial you'll need an active Microsoft Power BI subscription.

Before the information can be delivered to Power BI, it must be processed by a Azure Stream Analytics job.

  • Choose New > Internet of Things > Stream Analytics Job
  • Configure the Job, then click "Create"
  • Wait a couple of minutes until the Job has been created, then select All resources > name of your Stream Analytics Job
  • Click Inputs > Add

Set up input in the following way:

  • Input alias : data-from-tps
  • Source Type : Data stream
  • Source : IoT Hub
  • Subsriptiopn : Use IoT hub from current subscription
  • Endpoint : Messaging
  • Shared access policy name : iothubowner
  • Consumer group : powerbi
  • Click "Create"
Azure Stream Analytics:  Setting up Inputs
Azure Stream Analytics: Setting up Inputs

Set up output:

  • Output alias : data-to-powerbi
  • Click Otputs > Add
  • Choose Power Bi as sink
  • Click Authorize and enter your Power BI credentials in the appearing window
  • Enter Dataset Name and Table Name, e.g. "telemetry" and "environment", respectively
  • Click "Create"
Azure Stream Analytics:  Setting up Outputs
Azure Stream Analytics: Setting up Outputs

Now it's time to enter the query:

  • Click Query
  • Enter the following:

SELECT
AVG(humidity) AS humidity,
AVG(temperature) AS temperature,
AVG(pressure) AS pressure,
AVG(illumination) AS illumination,
System.Timestamp AS time,
IoTHub.ConnectionDeviceId AS deviceId
INTO
[data-to-powerbi]
FROM
[data-from-tps] TIMESTAMP by time
GROUP BY
TumblingWindow(Second, 60), IoTHub.ConnectionDeviceId


 

 

  • Click Save
Stream Analytics Query Language is a subset of SQL. Complete language documentation can be found here. There is also a very useful set of examples.
The query above, in short words, splits the timeline into 60-second periods and returns average values of humidity, temperature, pressure, and illumination for each period and each device.
  • Start your job
Azure Stream Analytics:  Writing the Query
Azure Stream Analytics: Writing the Query

 

Step 6: Visualizing your data
Open your Power BI workspace. Soon after you started the Stream Analytics job, a new dataset appears in the Navigation Bar. Report creation should not be a great challenge. Use "time" as Axis, "deviceId" as Legend and temperature/humidity/illumination/pressure as Value.

 

image

 

Step 7: Adding devices

  • Register second device as described in Step 3.
  • Upload and run code from Step 4 with modified connectionString value.

In short time the second curve appears in the report.

 

image

 

 

Made by Dmitry Slepov and Leonid Polyakov