Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Evolution of Printed Circuit Board Finishes - ENEPIG
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 26 Feb 2014 6:48 PM Date Created
  • Views 661 views
  • Likes 1 like
  • Comments 0 comments
  • finishes
  • pcb
  • Design
Related
Recommended

Evolution of Printed Circuit Board Finishes - ENEPIG

e14 Contributor
e14 Contributor
26 Feb 2014

The evolution of technology manufacturing is always moving towards a higher level of complexity. Newer designs have to be lighter, faster and smaller with every iteration of the next device. 

 

As a printed circuit board manufacturer, not only do we continue to move towards more complex technology but we strive to do so in an environmentally friendly way, working to eliminate potentially harmful chemicals from our processes.  To that end there have been recent advances and improvements to the surface finishes used on printed circuit boards.  The surface finish of the board is critical to how the components will connect and ultimately function in the final product.  The goal then is a surface finish that can accomplish strong connectivity and still meet today’s strict environmental demands.

 

We detail the most common surface finishes in another blog post called Printed Circuit Board Finishes.     There you will find information on the more common finish types including HASL, Lead Free HASL, ENIG, and more.  While you may be familiar with many of these, today we will introduce you to Electroless Nickel / Electroless Palladium / Immersion Gold (ENEPIG).

 

ENIG and Black Pad

 

ENIG has been a popular surface finish because of its very flat surface, ability to handle multiple reflow cycles and good shelf life.  However, there have been some challenges with ENIG because of nickel corrosion that can cause what is called "Black Pad". Black pad occurs when the nickel under the gold plating corrodes excessively and the component soldered to that pad loses connectivity.

 

ENIG can be challenging, as black pad can be difficult to detect when examining the surface finish since the gold completely covers the final surface.

 

Introduction to ENEPIG

 

Electroless Nickel / Electroless Palladium / Immersion Gold, or ENEPIG for short, has Palladium as one of the key ingredients. 

 

From Wikipedia:  Palladium is a chemical element with the chemical symbol Pd and an atomic number of 46. It is a rare and lustrous silvery-white metal discovered in 1803 by William Hyde Wollaston. 

 

While similar to Electroless Nickel Immersion Gold (ENIG) in process and application, the palladium in ENEPIG forms a flat, coplanar, hard surface with several advantages including gold wire bonding, aluminum wire bonding and excellent solderability, earning ENEPIG the nickname “the universal surface finish” (at least that’s what we call it!).  These advantages, along with a decrease in the price of palladium, have resulted in recent gains in popularity and demand for ENEPIG.

 

During the ENEPIG process, palladium is applied to the nickel before gold thus eliminating any problems with gold/nickel corrosion. By contrast, the ENIG process simply applies gold to the nickel.

Technical Stuff

 

IPC-4556 thickness specification states the following:

 

• All measurements should be done on a nominal pad size of 1.5 mm x 1.5 mm [0.060 in x 0.060 in] or equivalent area

• The EN thickness shall be 3-6 µm [118.1-236.2 µin] at ±4 sigma (standard deviations) from the mean

• The electroless Palladium (Pd) thickness shall be 0.05-0.15 µm [2-12 µin] at ±4 sigma (standard deviations) from the mean

• The minimum immersion Gold (Au) thickness shall be 0.025µm [1.2 µin] at -4 sigma (standard deviations) below the mean

 

Final Thoughts

 

Recent increases in gold costs and the demand for lead free finishes have driven improvements in the immersion gold processes for both ENIG and ENEPIG.  While ENEPIG has been around since the mid-90s, the cost, features, and advantages over ENIG have caused it to gain in recent popularity.

 

For those interested in diving deeper into the ENEPIG specifications, IPC has provided a detailed specification in the document “IPC-4556 Specification for ENEPIG” which can be purchased directly from IPC.  Additionally, there is a standards document (IPC-4552) available for ENIG that may be of interest.

 

For additional definitions of terms please visit our Printed Circuit Board Glossary of Terms page.

 

As always please comment and share and if you have any questions about your specific project please give us a call to discuss available options.