Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Exciting times as the NXP Freescale merger completes
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 10 Dec 2015 1:29 PM Date Created
  • Views 1339 views
  • Likes 1 like
  • Comments 5 comments
  • somnium
  • freescale
  • somniumdrt
  • kinetis
  • nxp
Related
Recommended

Exciting times as the NXP Freescale merger completes

e14 Contributor
e14 Contributor
10 Dec 2015

Here at SOMNIUM Technologies we're excited by the NXP Freescale merger which was finalized on Monday.

NXP is known as a pioneer in mixed signal technologies with recognized leadership in security. Freescale is recognized as a global leader in secure, embedded processing solutions. Freescale CEO Gregg Lowe noted that "the two companies have very complementary product portfolios and end market exposure, and this will enable us to offer better and more complete solutions to our customers." Certainly, it's anticipated that the newly merged organizations will be stronger together in addressing both the automotive and the IoT infrastructure market place, where industry standards are critical to success.

Both NXP and Freescale have long recognized the value of compatibility with industry standard GNU and Eclipse based solutions, and use these as the basis of their software enablement across their entire range of ARM Cortex M devices.

As a Freescale Proven Partner, and as the original developer of Freescale's Kinetis Design Studio IDE, we're excited about the merger.

Today we are announcing that DRT Freescale Kinetis IDE will be renamed as the DRT NXP Edition and will be extended to support NXP Cortex M devices. SOMNIUM DRT Kinetis IDE customers will be entitled to a free upgrade to the NXP version. This will allow even more developers to benefit from DRT's code optimization tools and enhanced Eclipse IDE, and shows the strength of DRT's roadmap to support market leading Cortex M devices.

In particular, NXPs focus on IoT and the automotive industry is one area where DRT unique benefits add significant value. It is these sectors which are being particularly challenged to use low cost smaller memory devices which use the least amount of energy, without any loss of performance, with many devices in the IoT space being solar powered or sealed for life battery based systems. This fits perfectly with DRT's sweet spot.

DRT is the only GNU compatible solution offering benefits over vanilla free of charge and other commercial GNU based tools. DRT reduces code size, improves performance and reduces energy consumption with no porting effort or source code changes required. DRT also uses an advanced Eclipse IDE, with features unavailable in other products to improve developer productivity and debugging.

As a result of the merger, the benefits that DRT brings to the embedded development world are now more widely available as we embrace the NXP development community. We look forward to working with NXP and its development community as we support NXP Cortex devices moving forward.

A free of charge, fully supported trial of SOMNIUM DRT is available here.

To be kept informed of DRT support for NXP's non-Kinetis devices please register here to join out mailing list.

  • Sign in to reply

Top Comments

  • COMPACT
    COMPACT over 10 years ago +2
    Nooooooooo! When it comes to technical documentation FreeScale deny any mistakes. I just hope this poor attitude does carry across with the merger.
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    Since you are advertising your product here you may as well respond to enquiries too:

     

    Does your product support ST Link, Keil Ulink2 and Keil Ulink Pro, Lauterbach uTrace. Does it support ETM debugging and if so does it at least match the Keil product for features (eg function timing, code coverage, os aware etc.).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    Hi Michael

     

    thanks for your interest in SOMNIUM DRT.  ST Link is in our pipeline for early 2016 and trace functionality is also something that we're actively developing.  We'd be keen to understand what you're working on and how we can help.  Would you be open to a direct call or email contact?

     

    Delyth

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to e14 Contributor

    You are welcome to email me (address is public just click on my name).

     

    Your response exposes the weakness in all the GCC/Eclipse based toolsets I've seen - no proper debugging - almost all high end Cortex M micros have the ETM on chip  but unless there is tool support it 's no use. How do people do serious work without proof of code coverage in testing ? How do they find the more recalcitrant bugs quickly without trace. You don't need these features all the time but when you do need them you really need them.

     

    If you were able to add competitive debugging (with Keil and IAR) it would make your tools a great deal more attractive.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 10 years ago in reply to e14 Contributor

    You are welcome to email me (address is public just click on my name).

     

    Your response exposes the weakness in all the GCC/Eclipse based toolsets I've seen - no proper debugging - almost all high end Cortex M micros have the ETM on chip  but unless there is tool support it 's no use. How do people do serious work without proof of code coverage in testing ? How do they find the more recalcitrant bugs quickly without trace. You don't need these features all the time but when you do need them you really need them.

     

    If you were able to add competitive debugging (with Keil and IAR) it would make your tools a great deal more attractive.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to michaelkellett

    We currently support the MTB in Cortex M0 devices. We started there partly because the optimization technology in our tools is of  particular benefit to people developing for devices with very limited memory. We are planning to add more advanced debugging support in future releases of DRT. Your input is useful as a pointer to the features we should look at.

    Jamie