Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Faster A to D for Arduino!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: YT2095
  • Date Created: 1 Mar 2012 11:07 AM Date Created
  • Views 682 views
  • Likes 1 like
  • Comments 1 comment
Related
Recommended

Faster A to D for Arduino!

YT2095
YT2095
1 Mar 2012

Having done a few blogs about A to D, D to A conversions, but focused mainly on the UNO32 board, I realised that I`v perhaps alienated a large chunk of people (very Naughty of me!), and so I`v turned my attention to the Arduino and it`s A to D audio capacities (or lack of without modification).

turns out it`s really quite simple as there`s no delay to mess about with unlike the UNO32 IDE.

for the Arduino it`s simply a case of altering the sample Prescaler, it`s default is set to 128, this is really rubbish! sorry and all that, but it is image

oddly there`s nothing in the Wiring_Analog.C file to alter unlike the Unos.

for the Arduino it`s in (here`s my pathway): Desktop\arduino-0022\hardware\arduino\cores\arduino  and then look for a file called "wiring.C"

again, as before Make a back-up of this file and hide it somewhere!

then open the original wiring.C file in Notepad, use full screen then scroll right the way down to the bottom, and look about a third of the way up and find:

 

#if defined(ADCSRA)

    // set a2d prescale factor to 128

    // 16 MHz / 128 = 125 KHz, inside the desired 50-200 KHz range.

    // XXX: this will not work properly for other clock speeds, and

    // this code should use F_CPU to determine the prescale factor.

    sbi(ADCSRA, ADPS2);

    sbi(ADCSRA, ADPS1);

    sbi(ADCSRA, ADPS0);

 

this little bit of code sets your prescaler, change the last 2 lines to:

 

sbi(ADCSRA, ADPS2);

cbi(ADCSRA, ADPS1);

cbi(ADCSRA, ADPS0);

 

yeah, you turn the `s` to a `c`, then save the file. and that`s it, you now have a prescaler of only 32 (4X faster).

this will work perfectly for simple Audio work with an R2R ladder D to A convertor, I use this Huge peice of code on my Arduino Nano as a simple pass-through:

 

void setup()              

{

  DDRD = B11111111;

}

void loop() {

  PORTD = (analogRead(0)>>1);   

}

 

digital pins D0 to D7 are used, LSB to MSB respectively.

 

although it is possible to take it faster, the results are likely to be flaky at best, I have yet to try this prog in ZED, where the 328p chips are running 25MHz (yes a genuine Atmel chip will go this fast, but you can forget serial coms etc...).

I`v also not tried this with PWM D to A either, in fact I`v never even tried PWM for anything yet other than servos.

also don`t panic about the fact that pins D0 and D1 (rx-tx) are used, if you built the R2R D to A with the 74HCT245 buffer chip as I did in mine a few blogs ago, the input impedance is so high, it`s completely ignored! and the fact your hitting PORT D will make no difference either, you can still upload and alter your programs via USB without having to pull 2 wires out every time image

 

so I hope I`m forgiven now for overlooking the Arduino community, I just get a bit carried away sometimes.

(Wife`s thinking; `I wish someone Would carry him away!`)

 

Have Phun image

  • Sign in to reply
  • fustini
    fustini over 14 years ago

    Interesting tip, I'll have to try when I need higher sampling speed.