Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs First of All, Tame the roaming beast, BBB AI.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fyaocn
  • Date Created: 11 Oct 2019 3:49 AM Date Created
  • Views 3467 views
  • Likes 10 likes
  • Comments 10 comments
  • visionthingch
Related
Recommended

First of All, Tame the roaming beast, BBB AI.

fyaocn
fyaocn
11 Oct 2019

Just got the BBB AI, But one should

Tame the roaming beast first.

image

Unlike normal BeagleBone_xx I used before, the BBB AI is one beast, roaming and heating instantly, then overheat tohalt.

But I like it. I know that is just what I want, as Nvidia GPU has done.

I am pretty sure TI is always good at performance balance, that is what TI can do at best. I would prepare to drive the BBB AI into water if neccessary.

I find one 80x80 CPU cooling fan now, it works fine. Of course,  25x25mm cooling fan would be better, I would place order.

 

But another problem comes, Tensorflow is only supported on 64bit OS. Unlike Raspberry Pi 3B+ and later which is 64bit compatible.

I shall find way out.

 

--------------------------

The 25x25x10 axis Fan arrives.

image

 

image

Looks OK, but I think it is WRONG ANSWER.

Why? Whatever the namerating of airflow or capacity, the center part is covered by the motor.

The test result proves my assumption. The BB-ai can work continuously even in heavy burden, but the temperature is obviously higher than my first ugly configuration. I think one Extention board BB AI cooling Addon board available by mayermakes  would be more practical choice.

The rim of fan blade offers more air flow. In this small 25x25 fan, the performance is poor.

I do not need quite CPU fan, but one noisy strong blow.

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +3
    That's a bit fan for a small board. Dubbie
  • mayermakes
    mayermakes over 7 years ago +3
    Hi in the meantime I have assembled and tested the first 0 batch of my BB-AI-Cooler addon board. and it works fine. I use it in a project to be seen on element14presents where the board is enclosed in…
  • fyaocn
    fyaocn over 7 years ago in reply to clem57 +2
    I have wrongly assumed so. Until I look up datasheet again, the hardware platform is 32 bit. I have been in Debian MIPS group. Debian is rich and diversity in nearly all types of hardware platform, while…
Parents
  • dubbie
    dubbie over 7 years ago

    That's a bit fan for a small board.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago

    That's a bit fan for a small board.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down