Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs First Steps with the Cypress BLE Pioneer Kit - Unboxing and BLE Sniffing
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 10 Apr 2015 10:43 AM Date Created
  • Views 2621 views
  • Likes 1 like
  • Comments 10 comments
  • bluetooth
  • ble
  • pioneer
  • cy8ckit-042
  • cypress_semiconductor
  • bluetooth_low_energy
  • bluetooth®
  • cypress
Related
Recommended

First Steps with the Cypress BLE Pioneer Kit - Unboxing and BLE Sniffing

Jan Cumps
Jan Cumps
10 Apr 2015

I'm a BLE beginner. Never developed anything for bluetoothRegistered, let alone the low energy variant.

I received a Bluetooth Low Energy Pioneer Kit ( cy8ckit-042-BLE ) yesterday. This blog is my story with the kits after a half day of testing.

 

image

 

What's Inside?

 

The kit contains four boards.

 

The USB Dongle

There's a USB dongle with a PRoC BLE chip. This is the part that you plug in your PC.

It's going to be one part of the BLE scenarios that you test out with this kit.

In the standard demo, it reacts on you poking the capacitive button on the Pioneer baseboard.

 

image

You can also interrogate this board with the Cypress software tools, query the attributes it received via BLE and send info from it over BLE.

The dongle pairs with the two BLE modules I show a bit further on.

 

The Pioneer Baseboard

That's the development board. The funny thing is that there's no BLE device on it. You have to plug in one of the two BLE modules that come with the kit. More on those two modules a bit later.

The Baseboard has your typical peripherals: debug module, some leds and buttons, even the Arduino compatible out-of-grid headers. But it doesn't have a programmable device on it.

 

image

 

The board acts as the host for the programmable modules, the:

 

Two BLE Modules

 

They are the focus of our exercises. We get two flavors:

PSoC: Programmable System-on-Chip

PRoC: Programmable Radio-on-Chip

Check this EE Times article for a quick-to-read background on them. http://www.eetimes.com/document.asp?doc_id=1324607

 

image

 

They can both be mounted on the Baseboard. That's when you get a fully functional development circuit.

 

 

The kit also includes some jumper wires, an USB cable, a battery and a quick start guide.

 

Software Install

 

Easy. I've chosen for the COMPLETE SETUP installation package,

That installs all the development tools, the kit info and examples, and the documentations.

After the install I updated all the packages to the latest version (there's an update wizard that helps with that.

As very last step, I made modifications to my Windows 8.1 setup, as explained in section 2.3: Windows 8.1 USB selective suspend setting of the KIT Guide.

Windows 8.1 default power profile makes USB go to sleep when idle. That powers off the dongle and your device stops working.

Following the few steps resolves that.

 

Out of the Box Demo

 

When you plug in the devices just like they are in the box, the dongle in one USB port, and the Baseboard with the PSoC BLE mounted, you get a working demo.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

You pair the dongle and BLE module by pushing the Button 2 on both devices.

The blue LED on the dongle will light up when they are connected.

 

You can then change that blue LED's intensity by swiping over the capacitive sensor on the Baseboard.

 

The PSoC BLE module sends the sensor value to the dongle via bluetooth, and the BLE Module acts on that by adapting the power sent to the LED.

The short video above show how that works. Note that the Baseboard is not connected to anything in that video. It's powered from the single coin cell underneath the board.

 

First Project

 

Well, that was really simple. I followed all the steps for section 4.2: CapSense Slider and LED of that sam KIT Guide.

That learns you how to build, load and debug the example, and also introduces the message attributes.

When you follow the example, you can log the changes in the capacitive sensor to a console,

and you'll also be able to change attributes.

You can tell the dongle to update a particular  attribute and send it to the BLE Module. That module will then make the RGB LED on the Baseboard light up in a particular color.


Summary

 

Everything worked straight out of the box. Big kudo's for that. I didn't loose a minute of my life troubleshooting the installation or the examples.

I could go straight into testing, and learned my first baby steps about bluetooth.

I'm still a beginner, but my first step on the learning ramp has been set.

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +2
    As for demo's you are right they just work. The CEO for Cypress is an engineer by trade and likes to take home the kits and test them out. They also insist on deliveromg full documentation with the software…
  • fvan
    fvan over 11 years ago in reply to clem57 +2
    It is indeed. The guy mentioned it during the workshop. It was even part of the workshop to flash it and use it as data generator
  • DAB
    DAB over 11 years ago +1
    Hi Jan, Yes, the Cypress kits are first rate and easy to use. I too have not done much with BLE so I will be following your progress with great interest. DAB
Parents
  • fvan
    fvan over 11 years ago

    I really like how this kit just works and contains everything you need to get started. Like Clem, I also followed the workshop. It was very well explained and gradually explored the many features the kit has to offer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to fvan

    BTW, the base for the kit imageI believe is same core as the 5LP image if you would like a preview for new PSoC 5LP

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago in reply to fvan

    BTW, the base for the kit imageI believe is same core as the 5LP image if you would like a preview for new PSoC 5LP

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • fvan
    fvan over 11 years ago in reply to clem57

    It is indeed. The guy mentioned it during the workshop. It was even part of the workshop to flash it and use it as data generator image