Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Getting Better with DC Motors
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 5 Jun 2019 10:21 AM Date Created
  • Views 711 views
  • Likes 10 likes
  • Comments 1 comment
  • dc motors
Related
Recommended

Getting Better with DC Motors

dubbie
dubbie
5 Jun 2019

In the recent Month of Robots competition I made something I called SuperRobot, but disapprovingly it wasn't so super as the DC motors and drivers I selected just didn't seem up to the task of moving the quite heavy chassis. I decided that I needed to get some better DC motors and gain a better understanding of the DC motor driver PCBs that are available for them. balearicdynamics recently illustrated some neat and small DC motors with metal gears and I thought they looked so good that I would get some myself to try out.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I plan to make a small four wheel driver mobile robot to see how good thy are, plus also how small I can make a mobile robot. I still have my TinyMobot (http://https://www.element14.com/community/people/dubbie/blog/2019/02/15/tinymobot-6-the-transparent-version) which I am playing with but that uses continuous rotation servo motors.

 

Dubbie

 

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +4
    Nice Dubbie! Note that there is also a thin shaft to the back of the motor (the part opposite to the reduction gearbox). It is a very interesting solution I think; this shaft rotates at the real RPM speed…
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Nice Dubbie!

     

    Note that there is also a thin shaft to the back of the motor (the part opposite to the reduction gearbox). It is a very interesting solution I think; this shaft rotates at the real RPM speed of the motor, no matter the reduction applied to the other side, and can be used to connect a rotary encoder for any kind of feedback. Using these motors with the Infineon Arduino DC motor controller shield, as well as with the micro:bit Kitronik's All-in-one robotics board, the speed is very stable when controlled with PWM frequency.

     

    Enrico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago

    Nice Dubbie!

     

    Note that there is also a thin shaft to the back of the motor (the part opposite to the reduction gearbox). It is a very interesting solution I think; this shaft rotates at the real RPM speed of the motor, no matter the reduction applied to the other side, and can be used to connect a rotary encoder for any kind of feedback. Using these motors with the Infineon Arduino DC motor controller shield, as well as with the micro:bit Kitronik's All-in-one robotics board, the speed is very stable when controlled with PWM frequency.

     

    Enrico

    • Cancel
    • Vote Up +4 Vote Down