The IoT Stamp module is powered by Realtek RTL8710AF ARM Cortex M3 WiFi SoC running at 83 MHz. This module features same form factor and GPIO layout as of ESP8266 but lacks ADC input.
But it features
Up to 1x SPI @ 41.5 Mbps max
Up to 3x UART with 2x up to 4Mbps, 1x @ 38400 bps
Up to 4x PWM
Up to 1x I2C @ 3.4 Mbps max
Up to 19 GPIOs including 10 supporting interrupts. And it comes with 1 MB of flash and 512 KB of RAM.
---------------------------------------------------------------------------------------------------
Used Commands:
AT
ATSR
ATSY
ATPW=1 //Station Mode
ATWS// Scan Wifi
ATPH=2,2// Mode AP 1/STA 2, Enable:DHCP 1/STATIC 2
ATPE=192.168.0.5// Static IP ATPN=weargenius,omisoksbwn// Connect to AP
ATW?// Wifi Info
ATPG=1 // Auto COnnect 0: Disable 1: Enable
ATPC=0,192.168.0.1,80 // Create TCp Client
ATPI// Connection Info
ATPT=70,1:"GET /tut/index.php?NAME=bikash /HTTP/1.1 Host:192.168.0.1:80\r\n"//Send Data
ATPR=1,20// rECEIVE dATA ATPD=0//0 FOR ALL OR conn_id
ATWD // Disconnect from AP
---------------------------------
Resources from Pine64 Website:
IOT Stamp Resources: http://bit.ly/2mNoxLT
Datasheet: http://bit.ly/2lOnYCj
Pinout Diagram: http://bit.ly/2mxGHR8
AT Commands guide: http://bit.ly/2mUtyT9
Getting Started Guide: http://bit.ly/2mwmYQc
********************************************************************
Subscribe YouTube : https://goo.gl/FhfdL7
Guys Subscribe to my channel for latest contents into your inbox.
Support me to keep going.
___________________________________________
Website : http://www.weargenius.in
Twitter : https://twitter.com/geekybikash
YouTube : https://www.youtube.com/weargenius
Instagram : https://www.instagram.com/weargenius/
GIT : https://github.com/oksbwn
Facebook: https://www.facebook.com/geekybikash
-
COMPACT
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
COMPACT
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children