Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Getting Started with the Cora Z7 Board - A Step by Step Guide to Creating the Vivado Project
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: adamtaylorcengfiet
  • Date Created: 4 Sep 2018 8:07 AM Date Created
  • Views 10059 views
  • Likes 5 likes
  • Comments 7 comments
  • xilinx_explore
  • cora z7
  • xilinx
  • digilent
Related
Recommended

Getting Started with the Cora Z7 Board - A Step by Step Guide to Creating the Vivado Project

adamtaylorcengfiet
adamtaylorcengfiet
4 Sep 2018

The Cora Z7 is a great development board for experienced developers and those who want to get started with FPGA’s. What makes the Cora Z7 ideal for this is that fact that is it a class of FPGA more correctly called a heterogeneous SoC, as the device combines a traditional FPGA with ARM processors. These two sections of the device are known as the programmable logic and the processing system respectively.

image

Cora Z7 board on the lab bench

This fusion of FPGA and Processor cores also means engineers who are perhaps more experienced with developing processor-based systems can also quickly and easily develop solutions using the ARM cores and Xilinx IP Library while they develop their Hardware Description Language Skills.

When it comes to the Cora board itself we get a range of popular interfaces such as Pmod and ChipKit / Shield connectors. These allow us to quickly and easily create solutions and we can use both the processors and the programmable logic to connect to them.

So, let’s look at how we can our first Cora Z7 design up and running quickly. Of course, the approach we are about to follow will be identical for any Zynq design.

The first thing we need to do is down download Vivado HLx to work with the CoraZ7 board and most other Zynq development boards the web pack version is sufficient. This comes with everything we need to develop both the programmable logic and the software we wish to run on the Zynq Processor core.

Once we have Vivado downloaded and installed the next stage is ensure Vivado is aware of the board we wish to develop with. This ensures Vivado is aware of the critical things such as the processor DDR configuration and the IO connections to the board. For Digilent boards we can down load the definitions from their Github. Once these files have been downloaded, they need to be installed in Vivado. Doing this is quick and simple copy the board definition files under the following path and restart Vivado

<Vivado Installation Path> data\boards\board_files

Once this is completed we can create our hardware description of the Zynq on the Cora Z7. In the Vivado design we create both the programmable logic contents and the configuration of the Zynq processors within the processing system.

image

Configuring the Zynq PS in Vivado

 

The first thing to do is create a project targeting the Cora Z7 board we just installed. Creating a project takes several steps via a project creation dialog.

With Vivado open the first step is to select ->project->new

 

image

This will open a project creation dialog which can be stepped through to configure the project as we desire. The first step is to define the project name and the location it is stored.

 

image

The next thee steps define the project type, which should be RTL project and allow you to add in any pre-existing RTL or constraints.

 

image

 

For this example, as we are starting from scratch we will not be adding any RTL or Constraints files.

image

The next stage of the project creation is to select the Cora Z7 development board from the list of boards Vivado is aware of.

 

image

 

Once the board has been selected this takes us to a project review page, clicking finish will create the project.

 

image

Developing solutions for the Zynq can be done visually using the IP integrator (IPI), this enables us to easily connect IP cores provided in the Vivado IP library. Of course, you can also package and add your own RTL cores to the design if you so desire as well.

To use IPI first need to create a block diagram to which we can add the IP we require, we do this by clicking on Create Block Design option beneath the IP integrator under Project Manager. This will open a Dialog asking about the block diagrams name and location. For this example leave them as the default and click OK.

 

image

This will create a blank template to which we can add IP from the Vivado IP Catalogue. To add IP we click on the on the add IP button on the menu, from the pop up dialog which appears the first thing we need to add in the Zynq processing system. In the search bar type Zynq and then add in the Zynq7 Processing System.

image

This will add in the Zynq processing system however, it will not be aware of the specific configuration needed for our Cora Z7 board. To configure the processing system for the Cora Z7 we must first run the block automation. Clicking on this will open a dialog, we do not need to make any changes for this application so click OK.

image

 

Once this has been completed we are ready to add in the rest of the design. For this design to demonstrate how to add in elements to the programmable logic and access them from the processing system. We are going to add in a BRAM controller and a BRAM which we can read or write from. This will demonstrate the techniques without the need for specific external modules or test equipment.

To add in the BRAM controller, click on the ADD IP button again, type BRAM in the search bar and select the AXI BRAM Controller.

image

 

Once the BRAM controller is added double clicking allows us to customise this controller. For this application we want to change the number of BRAM interfaces from two to one.

image

The final element of the design to add is the BRAM itself, again we do this using the ADD IP button.

image

Once both the BRAM and the BRAM Controller are present in the design, we need to connect them to the Zynq Processing system. We could do this by hand and insert the necessary reset and AXI interconnect structures. Alternatively, as we will do in this example leverage the connection automation wizard. Selecting this will open a dialog box, check the BRAM_PORTA and S_AXI on the left-hand side and click OK.

 

image

This will map in the AXI BRAM Controller and the BRAM into the Zynq memory space using the M_AXI_GP interface from the PS to the PL. The connection automation will also add in the necessary reset structure as well as connecting the clocks.

image

 

To see the processor system address range the BRAM has been mapped into, click on the address editor tab next to the Diagram tab. This will show you the address range and the memory size allocated.

image

Moving back to the block diagram the next step is to validate the design to ensure there are no issues with the design.

image

 

The first time validation is run, you may see a warning about the DDR timings, it is OK to work with the warning as such click OK.

image

With the block diagram create we need to convert the block diagram into the RTL files which can be synthesised and implemented to provide a bit stream.

Under the source tab select the bock diagram, right click and choose the option Create HDL Wrapper. This will create a HDL description of the top level of the design, whether this is VHDL or Verilog will depending upon your project language settings.

image

 

Selecting this option will generate a pop up, for now we can let Vivado manage this file. It will be re generated as we change the block diagram.

image

 

Once this is completed the next step is to generate the BIT file, clicking on the Generate Bitstream button will start the process. The first stage of this process will be to, synthesise each of the IP block used in the design before Synthesising the top level. Depending upon the power of your machine this may take some time.

image

 

Once the bit stream is completed, we can review the warnings and the device utilisation by looking at the project summary.

image

We are now in a position that we can begin to create our software application and test it on the board.

 

I will explain that in my next blog very soon.

  • Sign in to reply
  • angelo_
    angelo_ over 5 years ago in reply to michaelkellett

    Thank you Michael; i will try it... hoping that having two installations will not create problems...

     

    Still I don't think it's a good approach from Vivado, because this could mean that different version of the IDE will give different results with the same settings. On the long run this will create problems: imagine if you have a complex system and you need to debug something older...

     

    Anyway thank you again ... these are my first projects, so still a lot to learn!

     

    a.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to angelo_

    I don't know (not having used this board) but the Digilent examples will probably only work with the same version of Vivado that they were built for.

     

    They do warn about this on their website.

     

    I suggest you download the contemorary version and try that.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • angelo_
    angelo_ over 5 years ago

    Hi,

     

    I'm trying to execute the tutorial, but I continue to receive the following error:

     

    WARNING: [Vivado 12-818] No files matched 'myPath/Vivado/VIVADO-PROJECTS/Element14/Cora_e14/Cora_e14.gen/sources_1/bd/design_1/ip/design_1_blk_mem_gen_0_0/design_1_blk_mem_gen_0_0_ooc.xdc'

    ERROR: [Common 17-55] 'set_property' expects at least one object.

    Resolution: If [get_<value>] was used to populate the object, check to make sure this command returns at least one valid object.

     

    Please note that:

    I'm using

    Vivado 2020.2

    Ubuntu 18.04

    memory depth (auto) is 8192 instead of 2048,

    AXI BRAM 4.1 (instead of 4.0)

    target VHDL

     

    All the other logs seems ok.

     

    Somebody can help me? I'm a FPGA newbie ...

     

    Thank you in advance

     

    a.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adamtaylorcengfiet
    adamtaylorcengfiet over 8 years ago in reply to michaelkellett

    Should be all fixed now image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to adamtaylorcengfiet

    Great !

     

    Thanks.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>