Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Getting The Most Out Of Your Oscilloscope: Navigation With MAUI
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: caroline_teledynelecroy
  • Date Created: 14 Jun 2018 12:33 PM Date Created
  • Views 767 views
  • Likes 3 likes
  • Comments 0 comments
  • scope
  • teledyne
  • engineering
  • electronics
  • lecroy
  • maui
  • oscilloscope.
Related
Recommended

Getting The Most Out Of Your Oscilloscope: Navigation With MAUI

caroline_teledynelecroy
caroline_teledynelecroy
14 Jun 2018

Today's real-time digital oscilloscopes are easier to use than their predecessors, and new models get easier all the time. Oscilloscopes often are equipped with touch screens and elaborate user interfaces that provide a plethora of shortcuts and smartphone-like touch gestures that make common operations extremely fast and easy.

 

image

Figure 1: Oscilloscope UIs such as Teledyne LeCroy's MAUI provide tons of shortcuts and touch gestures

 

For example, Teledyne LeCroy's oscilloscopes with bandwidths of 200 MHz and higher are equipped with the MAUI with OneTouch user interface, which makes using an oscilloscope convenient, efficient, and intuitive. The UI performs all common operations with a single touch of the display using gestures you're used to from your phone, such as dragging, dropping, pinching, unpinching, and flicking. We'll discuss a few examples here.


For example, say you have Ch1 set up in a specific way and you want to duplicate that set up in Ch2. You'd simply touch and hold the descriptor box for Ch1 and drag and drop it onto the descriptor box for Ch2 (Figure 2). The same operation would serve to copy setups for math operations, zooms, and parameter measurements.

 

image

 

Figure 2: Copying a channel setup and duplicating it in another is a simple drag-and-drop gesture

 

Now, say you want to change the source for math operations, parameters, zooms, pass/fail tests, or triggers. Similar to how we duplicated a channel setup, we touch and hold the descriptor box for the item we want to change, and drag and drop it to the trigger descriptor box, or parameter of interest, and so on. You can also drag a channel descriptor box into the open dialog controls for, say, a math setup.

Next, here's how to Add New, with "New" being a channel, math operation, zoom trace, or memory. The Add New box is the area with a plus sign in it to the right of the channel descriptors on the display. You can touch that Add New box, which opens a dialog from which you can choose what New item you'd like. Or, drag a descriptor box onto the Add New button to create a new item.

 

image

Figure 3: Shown is an example of changing the source for a parameter measurement with a touch gesture


If you want to turn off a waveform trace or a parameter measurement, you simply "flick" it away by pushing it briskly toward the bottom of the touch screen. Cursors, which can be a challenge to deal with if you have multiple waveforms on the display, become easier with OneTouch. Underneath thetime base descriptors at bottom right of the display are cursor values. By touching, holding, and dragging those values to a waveform, the cursors are automatically placed on the grid at 2.5 divisions from the left and right and 7.5 divisions down from the top of the grid.

There are more general uses for gestures, too, as well as multi-touch gestures. You can use a fingertip and thumb to pinch or unpinch a waveform to zoom in or out. Waveforms can be dragged right or left within a grid to adjust their horizontal positioning or up or down for vertical positioning. You can also drag a finger diagonally across a waveform to create a new zoom of a section of interest. Nearly everything on the MAUI with OneTouch UI can be dragged.

 

image

 

Figure 4: Pinch/unpinch traces to zoom in or out (top), drag waveforms to reposition them (center), or drag diagonally to create a new zoom trace (bottom)

 

Sometimes it's easier to show something than to describe it, so to that end, we've created a series of 10 short videos about MAUI with OneTouch. Take a look if you haven't seen the UI in action.

 

In our next post, we'll cover a couple of handy tips for setting the preferences in your oscilloscope.

 

Previous posts in this series:

Getting The Most Out of Your Oscilloscope: Setup