Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs HDC1000EVM communications protocol
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wymand
  • Date Created: 18 Apr 2015 11:43 PM Date Created
  • Views 2238 views
  • Likes 1 like
  • Comments 9 comments
Related
Recommended

HDC1000EVM communications protocol

wymand
wymand
18 Apr 2015

Having been in communications since 1962 when NSA recruited me into the Army Security agency and my career after that

as a consultant, WSP communications engineering, WSDOT, and WSCTC consultant, I am particularly interested in how devices talk

So, lacking any reply from TI to questions on protocol, I am looking for myself.

 

The following Program is not intended to be fancy but gives out some communications protocol

that TI has not published yet!  TI has stated their intent to publish the full communications protocol

for the MSP230 communication with the i2c.  As written it works on my RPi B 


import serial

import binascii

#sample program to read Texas Instruments HDC1000EVM

#initialization and open the port

#possible timeout values:

 

 

#    1. None: wait forever, block call

#    2. 0: non-blocking mode, return immediately

#    3. x, x is bigger than 0, float allowed, timeout block call

ser = serial.Serial()

 

 

#ser.port = "/dev/ttyUSB0"

#ser.port = "COM4:"

#ser.port = "/dev/ttyACM1"

ser.port = "/dev/serial/by-path/platform-bcm2708_usb-usb-0:1.2:1.0"

ser.baudrate = 115200

ser.bytesize = serial.EIGHTBITS #number of bits per bytes

ser.parity = serial.PARITY_NONE #set parity check: no parity

ser.stopbits = serial.STOPBITS_ONE #number of stop bits

#ser.timeout = None          #block read

#ser.timeout = 1           #non-block read

ser.timeout = 2              #timeout block read

ser.xonxoff = False     #disable software flow control

ser.rtscts = False     #disable hardware (RTS/CTS) flow control

ser.dsrdtr = False       #disable hardware (DSR/DTR) flow control

ser.writeTimeout = 2     #timeout for write

 

 

try:

    ser.open()

except Exception as e:

    print ("error open serial port: " + str(e))

    exit()

if ser.isOpen():

    try:

        ser.flushInput() #flush input buffer, discarding all its contents

        ser.flushOutput()#flush output buffer, aborting current output

                        #and discard all that is in buffer

        #write data

 

 

        ser.write(serial.to_bytes([0x4C,0x12,0x01,0x00,0x03,0x40,0xFB,0x02,0x7a]))

        response = ser.readline()

        print("read Serial Number MSB = : 0x" + str(binascii.hexlify(response[7])) + str(binascii.hexlify(response[8])))

 

 

        ser.write(serial.to_bytes([0x4C,0x12,0x01,0x00,0x03,0x40,0xFc,0x02,0x11]))

        response = ser.readline()

        print("read Serial Number MID = : 0x" + str(binascii.hexlify(response[7])) + str(binascii.hexlify(response[8])))

 

 

        ser.write(serial.to_bytes([0x4C,0x12,0x01,0x00,0x03,0x40,0xFd,0x02,0x04]))

        response = ser.readline()

        print("read Serial Number LSB = : 0x" + str(binascii.hexlify(response[7])) + str(binascii.hexlify(response[8])))

 

 

        ser.write(serial.to_bytes([0x4C,0x12,0x01,0x00,0x03,0x40,0xFe,0x02,0x3b]))

        response = ser.readline()

        print("read Manufacturer = :" + str(response[7]) + str(response[8]))

 

 

        ser.write(serial.to_bytes([0x4C,0x12,0x01,0x00,0x03,0x40,0xFF,0x02,0x2e]))

        response = ser.readline()

        print("read Device ID = : 0x" + str(binascii.hexlify(response[7])) + str(binascii.hexlify(response[8])))

 

 

        ser.write(serial.to_bytes([0x33]))

        numOfLines = 0

        while True:

            response = ser.readline()

            if (str(response).find(",") == -1):

                print("start data: " + str(response))

            else:

                print("      Temperature: " + str(("{0:.2f}".format(((float(int((str(response).split(',')[0]),16))/float(65536)) * 165) -40)))+ u"\u00B0" + "C")

                print("      Temperature: " + str(("{0:.2f}".format((((((float(int((str(response).split(',')[0]),16))/float(65536)) * 165) -40) * 9) / 5) + 32)))+ u"\u00B0" + "F")

                print("Relative Humidity: " + str(("{0:.2f}".format((float(int((str(response).split(',')[1]),16))/float(65536)) * 100)))+ "%")

            numOfLines = numOfLines + 1

            if (numOfLines > 10):

                #ser.write(bytes(44))

                ser.write(serial.to_bytes([0x34]))

                response = ser.readline()

                print("read data: " + str(response))

                break

                ser.close()

    except Exception as e1:

        print ("error " + str(e1))

    #ser.write(bytes(44))

    ser.write(serial.to_bytes([0x34]))

    response = ser.readline()

    print("last data: " + str(response))

    ser.close()

else:

    print ("cannot open serial port ")

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +2
    I like what you have done here. Helps the guys who know code to do very interesting things, Thanks, Clem
  • mcb1
    mcb1 over 11 years ago +1
    Doug For those of us who are not so software literate, how do you use it in a RPi. I'm assumming it is python .... Mark
  • wymand
    wymand over 11 years ago in reply to mcb1 +1
    Mark, Yes, it is python. save the program with a name ending in .py I used hdc1000.py Then, in a terminal window type python hdc1000.py and it should locate the port that the HDC1000EVM is connected on…
Parents
  • michaelwylie
    michaelwylie over 11 years ago

    Doug;

     

    For verification here is the result of your script, modified for the serial address, running on the Pi 2:

     

     

    read Serial Number MSB = : 0x01e4

    read Serial Number MID = : 0xea14

    read Serial Number LSB = : 0x6d00

    read Manufacturer = :TI

    read Device ID = : 0x1000

    start data: stream start

     

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.26°C

          Temperature: 73.88°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.26°C

          Temperature: 73.88°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

    read data: stream stop

     

    last data: stream stop

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelwylie
    michaelwylie over 11 years ago

    Doug;

     

    For verification here is the result of your script, modified for the serial address, running on the Pi 2:

     

     

    read Serial Number MSB = : 0x01e4

    read Serial Number MID = : 0xea14

    read Serial Number LSB = : 0x6d00

    read Manufacturer = :TI

    read Device ID = : 0x1000

    start data: stream start

     

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.26°C

          Temperature: 73.88°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.26°C

          Temperature: 73.88°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

          Temperature: 23.25°C

          Temperature: 73.86°F

    Relative Humidity: 44.29%

    read data: stream stop

     

    last data: stream stop

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • wymand
    wymand over 11 years ago in reply to michaelwylie

    Mike,

      Thanks for the verification.  It helps to know that it runs on more than just my Pi.