Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs HDC1000EVM Python code for Raspberry Pi
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wymand
  • Date Created: 16 Apr 2015 12:08 AM Date Created
  • Views 1157 views
  • Likes 1 like
  • Comments 4 comments
  • python
  • hdc1000evm
  • raspberry-pi
Related
Recommended

HDC1000EVM Python code for Raspberry Pi

wymand
wymand
16 Apr 2015

Here is a sample program that starts a stream from the HDC1000EVM, reads 100 returns and  stops the stream:

 

import serial

#sample program to read Texas Instruments HDC1000EVM

#initialization and open the port

#possible timeout values:

 

 

#    1. None: wait forever, block call

#    2. 0: non-blocking mode, return immediately

#    3. x, x is bigger than 0, float allowed, timeout block call

ser = serial.Serial()

 

 

#ser.port = "/dev/ttyUSB0"

#ser.port = "COM4:"

#ser.port = "/dev/ttyACM1"

ser.port = "/dev/serial/by-path/platform-bcm2708_usb-usb-0:1.2:1.0"

ser.baudrate = 115200

ser.bytesize = serial.EIGHTBITS #number of bits per bytes

ser.parity = serial.PARITY_NONE #set parity check: no parity

ser.stopbits = serial.STOPBITS_ONE #number of stop bits

#ser.timeout = None          #block read

#ser.timeout = 1           #non-block read

ser.timeout = 2              #timeout block read

ser.xonxoff = False     #disable software flow control

ser.rtscts = False     #disable hardware (RTS/CTS) flow control

ser.dsrdtr = False       #disable hardware (DSR/DTR) flow control

ser.writeTimeout = 2     #timeout for write

 

 

try:

    ser.open()

except Exception as e:

    print ("error open serial port: " + str(e))

    exit()

if ser.isOpen():

    try:

        ser.flushInput() #flush input buffer, discarding all its contents

        ser.flushOutput()#flush output buffer, aborting current output

                        #and discard all that is in buffer

        #write data

        #ser.write(bytes(43))

        ser.write(serial.to_bytes([0x33]))

        numOfLines = 0

        while True:

            response = ser.readline()

            if (str(response).find(",") == -1):

                print("start data: " + str(response))

            else:

                print("      Temperature: " + str(("{0:.2f}".format(((float(int((str(response).split(',')[0]),16))/float(65536)) * 165) -40)))+ u"\u00B0" + "C")

                print("      Temperature: " + str(("{0:.2f}".format((((((float(int((str(response).split(',')[0]),16))/float(65536)) * 165) -40) * 9) / 5) + 32)))+ u"\u00B0" + "F")

                print("Relative Humidity: " + str(("{0:.2f}".format((float(int((str(response).split(',')[1]),16))/float(65536)) * 100)))+ "%")

            numOfLines = numOfLines + 1

            if (numOfLines >= 100):

                #ser.write(bytes(44))

                ser.write(bytes(52))

                response = ser.readline()

                print("read data: " + str(response))

                break

                ser.close()

    except Exception as e1:

        print ("error " + str(e1))

    ser.write(serial.to_bytes([0x34]))

    response = ser.readline()

    print("last data: " + str(response))

    ser.close()

else:

    print ("cannot open serial port ")

  • Sign in to reply
Parents
  • wymand
    wymand over 11 years ago

    In case it hasn't been noticed, the RPi code uses byte(43) to initiate the stream and byte(44) to stop the stream.  Now I don't know why *yet* but the protocol for starting a stream is definitely a "3" or decimal character 51 (hex 0x33)  and stopping the stream is definitely a "4" decimal 52 (hex 0x34) I want to make this clear because my next blog entry is going to look at the communications protocol that is used to address the device. I will be doing this on my PC because that is where all my tools are located.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • wymand
    wymand over 11 years ago

    In case it hasn't been noticed, the RPi code uses byte(43) to initiate the stream and byte(44) to stop the stream.  Now I don't know why *yet* but the protocol for starting a stream is definitely a "3" or decimal character 51 (hex 0x33)  and stopping the stream is definitely a "4" decimal 52 (hex 0x34) I want to make this clear because my next blog entry is going to look at the communications protocol that is used to address the device. I will be doing this on my PC because that is where all my tools are located.