Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Helical Copper Tape Antenna for 2m
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kmikemoo
  • Date Created: 4 Feb 2021 3:51 AM Date Created
  • Views 6438 views
  • Likes 8 likes
  • Comments 3 comments
  • antenna
  • ham radio
  • amateur radio
Related
Recommended

Helical Copper Tape Antenna for 2m

kmikemoo
kmikemoo
4 Feb 2021

What can I say?  I like projects that involve PVC.  That way, when I goof it up, it's not expensive to redo.

This antenna was created by John Portune, W6NBC, and it was featured by the ARRL in QST (their magazine) and on a webinar.  You can also find it on John's webpage.

https://w6nbc.com/articles/20xx-QSTcopperhelixantenna.pdf

 

As John describes it, it's a combination (slightly) off-center fed dipole and (continuously loaded) loading coil.  What intrigues me is that it's a dipole that's shorter than 1/4 wavelength.  Of course, mine aren't - but a spartan model could be.  And it's advertised to have 1.64dBi of gain.  Not bad.

image

This antenna has been assembled so sit atop a 1" PVC mast.  The thin white tube is a piece of PEX epoxied into two 3/4" PVC caps.  This ensures the feed line is centered in the 1-1/4" PVC tube - and through the bottom half of the dipole.  I didn't get it up before the snow came so it will have to wait another couple of months.  I have tested it out using packet radio and the transmissions went through just fine.

 

image

This is essentially the same antenna but this one was built for a hidden transmitter hunt.  Interesting to note was that painting the copper tape moved the resonant frequency 2 MHz from 147.5 MHz to 145.3 MHz.  I have heard that painting an antenna doesn't change its characteristics much, but the 2 meter band is only 4 MHz wide.  I guess the phrase "much" is fairly subjective.

 

All in, these were fun and simple to build.  I still haven't decided if the next iteration will be for 440 MHz or 915 MHz.  I'll probably need some thinner copper tape.

  • Sign in to reply

Top Comments

  • phoenixcomm
    phoenixcomm over 5 years ago +3
    Mike Moore's Blog very cool, Mr Mike! ~~Cris
  • shabaz
    shabaz over 5 years ago +3
    Hi Mike, Very well built antenna! I can imagine such a style antenna is very easy to make rugged and weather-resistant as you've shown, with paint or tape etc. Nice design!
  • kmikemoo
    kmikemoo over 5 years ago in reply to phoenixcomm +2
    Thanks, Cris! The next iteration is going to be a 915MHz version for an Arduino LoRa shield.
Parents
  • phoenixcomm
    phoenixcomm over 5 years ago

    Mike Moore's Blog very cool, Mr Mike!

    ~~Cris

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 5 years ago

    Mike Moore's Blog very cool, Mr Mike!

    ~~Cris

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kmikemoo
    kmikemoo over 5 years ago in reply to phoenixcomm

    Thanks, Cris!  The next iteration is going to be a 915MHz version for an Arduino LoRa shield.