Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs how to know which serial node is mapped with hardware  processor UART pins
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 14 Nov 2014 11:23 AM Date Created
  • Views 762 views
  • Likes 0 likes
  • Comments 0 comments
  • uart_interface
  • imx6q
Related
Recommended

how to know which serial node is mapped with hardware  processor UART pins

e14 Contributor
e14 Contributor
14 Nov 2014

Hello All,

 

 

                I am working on IMX6 based processor which have 5 UART pins/port coming out of it. There are 4 nodes in /dev folder for serial ports i.e ttymxc1,ttymxc2,ttymxc3,ttymxc4 and i want to know which node is mapped with which hardware UART. I have console enabled on ttymxc1 through which i can see logs. I want to perform read and write on serial port by using node other than ttymxc1 i.e from  ttymxc2,ttymxc3,ttymxc4.

 

I have found something during boots as give below

 

   1.378111] mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver lcd

[    1.463018] Console: switching to colour frame buffer device 30x20

[    1.513646] imx-sdma imx-sdma: loaded firmware 1.1

[    1.530828] imx-sdma imx-sdma: initialized

[    1.539131] Serial: IMX driver

[    1.542435] imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX

[    1.548934] console [ttymxc1] enabled, bootconsole disabled

[    1.548934] console [ttymxc1] enabled, bootconsole disabled

[    1.560731] imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

[    1.567762] imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX

[    1.574861] imx-uart.4: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX

[    1.593302] loop: module loaded

[    1.596531] at24 0-0050: 256 byte at24 EEPROM, writable, 16 bytes/write

[    1.603253] at24 0-0051: 256 byte at24 EEPROM, writable, 16 bytes/write

[    1.609969] at24 1-0050: 256 byte at24 EEPROM, writable, 16 bytes/write

[    1.616626] at24 1-0051: 256 byte at24 EEPROM, writable, 16 bytes/write

 

 

Help me asap.

 

Thanks

 

Jai Prakash