Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Hydrogen Fuel Cell.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Muju4mFrnL
  • Date Created: 7 Oct 2009 10:15 AM Date Created
  • Views 794 views
  • Likes 0 likes
  • Comments 0 comments
  • renewable_source
  • fuel_cell
  • cell
  • power
  • hydrogen_for_power
Related
Recommended

Hydrogen Fuel Cell.

Muju4mFrnL
Muju4mFrnL
7 Oct 2009

Fuel cells can possibly power any thing from tiny microchips to car and power plants.

 

What is a fuel cell?

A fuel cell is a device that generates  electricity by a chemical reaction. Every fuel cell has two electrodes, one positive  and one negative, called, respectively, the anode and cathode. The reactions that  produce electricity take place at the electrodes.

Every fuel cell also has an electrolyte, which carries electrically charged particles  from one electrode to the other, and a catalyst, which speeds the reactions at the  electrodes.

Hydrogen is the basic fuel, but fuel cells also require oxygen. One great appeal of  fuel cells is that they generate electricity with very little pollution—much of the  hydrogen and oxygen used in generating electricity ultimately combine to form a  harmless byproduct, namely water.

One detail of terminology: a single fuel cell generates a tiny amount of direct  current (DC) electricity. In practice, many fuel cells are usually assembled into a  stack. Cell or stack, the principles are the same.

 

 

How do fuel cells work?

The purpose of a fuel cell is to produce an electrical current that can be directed  outside the cell to do work, such as powering an electric motor or illuminating a  light bulb or a city. Because of the way electricity behaves, this current returns to  the fuel cell, completing an electrical circuit. (To learn more about electricity and  electric power, visit “Throw The Switch” on the Smithsonian website Powering a  Generation of Change.) The chemical reactions that produce this current are the key  to how a fuel cell works.

There are several kinds of fuel cells, and each operates a bit differently. But in  general terms, hydrogen atoms enter a fuel cell at the anode where a chemical reaction  strips them of their electrons. The hydrogen atoms are now “ionized,” and carry a  positive electrical charge. The negatively charged electrons provide the current  through wires to do work. If alternating current (AC) is needed, the DC  output of the fuel cell must be routed through a conversion device called an  inverter.

animated image showing the function of a PEM  fuel cell
Graphic by Marc Marshall, Schatz  Energy Research Center

Oxygen enters the fuel cell at the  cathode and, in some cell types (like the one illustrated above), it there combines  with electrons returning from the  electrical circuit and hydrogen ions that have traveled through the electrolyte from  the anode. In other cell types the oxygen picks up electrons and then travels through  the electrolyte to the anode, where it combines with hydrogen ions.

The electrolyte plays a key role. It must permit only the appropriate ions to pass  between the anode and cathode. If free electrons or other substances could travel  through the electrolyte, they would disrupt the chemical reaction.

Whether they  combine at anode or cathode, together hydrogen and oxygen form water, which drains  from the cell. As long as a fuel cell is supplied with hydrogen and oxygen, it will  generate electricity.

Even better, since fuel cells create electricity chemically, rather than by combustion,  they are not subject to the thermodynamic laws that limit a conventional power plant  (see “Carnot Limit” in the glossary). Therefore, fuel cells are more efficient in  extracting energy from a fuel. Waste heat from some cells can also be harnessed,  boosting system efficiency still further.

 

For more details one can visit the link below.

 

http://americanhistory.si.edu/fuelcells/basics.htm