Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs ICL8038 waveform generator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinvalencia
  • Date Created: 17 Mar 2015 4:17 PM Date Created
  • Views 3444 views
  • Likes 6 likes
  • Comments 7 comments
  • board
  • oscillators
  • waveforms
  • sin
  • frecuency
  • square
  • icl8038
Related
Recommended

ICL8038 waveform generator

martinvalencia
martinvalencia
17 Mar 2015

The ICL8038 waveform generator is a monolithic integrated circuit capable of producing high accuracy sine, square, triangular, sawtooth and pulse waveforms with a minimum of external components. The frequency (or repetition rate) can be selected externally from 0.001Hz to more than 300kHz using either resistors or capacitors, and frequency modulation and sweeping can be accomplished with an external voltage.(Datasheet ICL8038)...Obsolete product but  only use for students

 

ICL8038 Data

 

Internal diagram of the oscillator

image

According to the data sheet can be used with two power supplies and a single power supply.

In my application Use only one power supply (12V), consumption of integrated circuit is very low (less than 20mA)

 

Circuit diagram implemented

image

Board

image

Printed circuit implemented

IMG_20150307_143506754.jpgelectronaplica20150307152441568.jpg

 

 

 

 

 

 

 

 

 

 

 

 

IMG_20150307_151856219.jpg

 

Capture Oscilloscope - forms of signals

 

singal1.png

singal2.png

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    I like it. Everyone needs a simple waveform generator now and then. It looks like you have a good one. DAB
  • jw0752
    jw0752 over 11 years ago +1
    Hi Martin, I was first introduced to the ICL8038 chip by an Excellent on line tutorial site "Electronic Tutorials" http://www.electronics-tutorials.ws/waveforms/waveforms.html It is a shame that this chip…
  • peterjcs23
    peterjcs23 over 11 years ago +1
    Hi Martin, Analog Devices make waveform synthesis chips AD5932 and AD5930. They are modern digitally controlled chips. I've never used one but they are worth a look, if you want to check out an Arduino…
  • martinvalencia
    martinvalencia over 11 years ago in reply to DAB

    hehehe you have reason, I had to assemble a signal generator because it was necessary for different applications, so that implements a simple one image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 11 years ago

    I like it.

     

    Everyone needs a simple waveform generator now and then.

     

    It looks like you have a good one.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<