Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs ICL8038 waveform generator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinvalencia
  • Date Created: 17 Mar 2015 4:17 PM Date Created
  • Views 3482 views
  • Likes 6 likes
  • Comments 7 comments
  • board
  • oscillators
  • waveforms
  • sin
  • frecuency
  • square
  • icl8038
Related
Recommended

ICL8038 waveform generator

martinvalencia
martinvalencia
17 Mar 2015

The ICL8038 waveform generator is a monolithic integrated circuit capable of producing high accuracy sine, square, triangular, sawtooth and pulse waveforms with a minimum of external components. The frequency (or repetition rate) can be selected externally from 0.001Hz to more than 300kHz using either resistors or capacitors, and frequency modulation and sweeping can be accomplished with an external voltage.(Datasheet ICL8038)...Obsolete product but  only use for students

 

ICL8038 Data

 

Internal diagram of the oscillator

image

According to the data sheet can be used with two power supplies and a single power supply.

In my application Use only one power supply (12V), consumption of integrated circuit is very low (less than 20mA)

 

Circuit diagram implemented

image

Board

image

Printed circuit implemented

IMG_20150307_143506754.jpgelectronaplica20150307152441568.jpg

 

 

 

 

 

 

 

 

 

 

 

 

IMG_20150307_151856219.jpg

 

Capture Oscilloscope - forms of signals

 

singal1.png

singal2.png

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    I like it. Everyone needs a simple waveform generator now and then. It looks like you have a good one. DAB
  • jw0752
    jw0752 over 11 years ago +1
    Hi Martin, I was first introduced to the ICL8038 chip by an Excellent on line tutorial site "Electronic Tutorials" http://www.electronics-tutorials.ws/waveforms/waveforms.html It is a shame that this chip…
  • peterjcs23
    peterjcs23 over 11 years ago +1
    Hi Martin, Analog Devices make waveform synthesis chips AD5932 and AD5930. They are modern digitally controlled chips. I've never used one but they are worth a look, if you want to check out an Arduino…
  • peterjcs23
    peterjcs23 over 11 years ago in reply to martinvalencia

    Farnell stock the AD5930, if you have an account, or I think you can use a credit card. Peter

    http://uk.farnell.com/analog-devices/ad5930yruz/ic-waveform-generator-25mhz-tssop/dp/1274252?ost=AD5930

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 11 years ago in reply to peterjcs23

    AD5930 is an interesting device, I wasn't aware of such a device also has a high operating frequency; i'll try to find it in my country, thanks for the info

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • peterjcs23
    peterjcs23 over 11 years ago

    Hi Martin, Analog Devices make waveform synthesis chips AD5932 and AD5930. They are modern digitally controlled chips. I've never used one but they are worth a look, if you want to check out an Arduino or RasPi project...Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinvalencia
    martinvalencia over 11 years ago in reply to jw0752

    thank you very much for the link and it really is a shame that this chip is out of service, I see really useful in many ways, I hope to have a more modern version, will inquire a little about their new versions image

     

    Regards

     

    Martin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago

    Hi Martin,

    I was first introduced to the ICL8038 chip by an Excellent on line tutorial site "Electronic Tutorials"

    http://www.electronics-tutorials.ws/waveforms/waveforms.html

    It is a shame that this chip is out of production as it is very flexible and fun to work with. You did a very nice job making a board and demonstrating it. Thanks for the great post.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>