Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs indian economy
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mandeep11904
  • Date Created: 4 Dec 2016 4:00 PM Date Created
  • Views 1020 views
  • Likes 3 likes
  • Comments 1 comment
Related
Recommended

indian economy

mandeep11904
mandeep11904
4 Dec 2016

India needs a Rs.200 note, not a Rs.2,000 note and the science behind it

Ravi Abhyankar/01 December 2016

What should be the size of the Apple Mac screen? Technically, Apple can produce hundreds of different sizes, but they have settled on four: 13.3 inch, 15.4 inch, 21.5 inch, and 27 inch. The four are spaced close enough, and far enough to satisfy most Apple consumers.

Industrial design has a mathematical concept called preferred numbers. Way back in 1870s, a French engineer Charles Renard proposed a system based on logarithmic scale to produce a limited number of sizes to cover a wide range. A variant of that internationally accepted system is the 1-2-5 series, which is widely used in minting coins and printing notes.

The 1, 2, 5, 10, 20, 50, 100, 200, 500, 1000… is that series. The beauty of the series is that any adjacent numbers differs by a product of 2 or 2.5. As a result, they are spaced close enough but cover a wide ground. How? Let us look at an Indian street vendor who still measures the fruit he sells on old-fashioned scales. If he has weights of 100gms, 200gms, 500gms and 1 kg, he can give you fruits in multiples of 100gms by using a maximum of three weights. E.g. 800 (500+200+100), 900 (500+200+200). In no case does the seller need to use four weights. If you must follow the decimal system, this is an extremely efficient system.

Now look at the Indian banknotes. Until 8 November 2016, India had currency (notes or coins) with a denomination of 1, 2, 5, 10, 20, 50, 100, 500 and 1000 rupees. Below Rs100, transactions were efficient. The gap between Rs100 and Rs500 (1:5) has been too large. Over the last few years, it has produced inconvenience (certainly) and contributed to inflation (probably). It is well known that bigger values and larger gaps can increase prices. In January 2002, when most European currencies converted to Euro, prices rose on many goods as a result of rounding up. This rounding up phenomenon has made coins below one rupee disappear from India.

I had hoped that Reserve Bank of India (RBI) would use the demonetization to introduce a Rs200 note. That would have bridged the gap between Rs100 and Rs500 and made the cash economy efficient. What we got instead was a Rs2,000 note.

With the death of the Rs1,000 note, the new ratio of Rs500-Rs2,000 (1:4) to follow the already inefficient Rs100- Rs500 (1:5) is not sustainable, now or in future. And since the new Rs500 note is as yet rarely available, the ratio currently is Rs100-Rs2000 (1:20). When the maximum prescribed ratio for efficiency is 1:2.5, in practice we have 1:20, which is catastrophic. That is why; we have millions of people with wads of Rs2,000 notes unable or unwilling to make a small purchase of Rs200.

This is pure and simple mathematical illiteracy. I expect the Reserve Bank to be aware of the Renard series, which is an ISO standard. Politics and economics can be subject to opinions, but not mathematics. You invite disaster when you do not follow the basic number rules.

What India needs to do urgently is to introduce an Rs200 note. And if Rs1,000 is to be permanently abandoned, then to withdraw Rs2,000 as well. For efficient transactions, the ratio in the 1-2-5 series must never exceed 2.5.

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago +1
    This has nothing to with E14 but is interesting. In the UK the change was widely reported as an anti corruption measure and actually intended to make cash transactions more difficult and to force large…
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    This has nothing to with E14 but is interesting.

     

    In the UK the change was widely reported as an anti corruption measure and actually intended to make cash transactions more difficult and to force large collections of cash to be cycled through the banking system and so revealed to the authorities.

     

    I suspect that your suggestion of logically based banknote values is far too sensible for it to have any appeal to politicians.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 9 years ago

    This has nothing to with E14 but is interesting.

     

    In the UK the change was widely reported as an anti corruption measure and actually intended to make cash transactions more difficult and to force large collections of cash to be cycled through the banking system and so revealed to the authorities.

     

    I suspect that your suggestion of logically based banknote values is far too sensible for it to have any appeal to politicians.

     

    MK