Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs JFET Colpitts Oscillator
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 9 Jan 2021 10:54 PM Date Created
  • Views 9203 views
  • Likes 10 likes
  • Comments 3 comments
  • colpitts
  • oscillator
  • jfet
  • bf256b
  • analogue
  • jc2048
Related
Recommended

JFET Colpitts Oscillator

jc2048
jc2048
9 Jan 2021

Introduction

 

This one started last year with me just messing around on a windy, rain-swept day, seeing if I could do something

simple with a JFET. It's taken quite a while to make it to the blog: I dropped it, started it again, stalled, and

have now, eventually, finished it. [It was also leap-frogged by the regulator-as-an-oscillator one, which you'll

notice had quite a lot in common with this one.]

 

What I was trying for was an oscillator that had an output frequency of several hundred kilohertz and where the

frequency could be varied by perhaps 10kHz or so by adding a modest amount of capacitance, say up to about 50pF

max. Take note that I don't really know what I'm doing with all this analogue stuff, so don't read it as a tutorial

because, whatever it is, it's certainly not that. Comments are welcome, particularly if you can tell me how I

should be doing this.

 

For the gain element I'm going to use a JFET. That's because this is a follow-on from some of the JFET blogs I did

a little while back and I'm currently interested in how they work. I've used a BF256BBF256B n-channel part simply because

I have some. According to the datasheet, that part was originally 'designed for VHF/UHF amplifiers' so it shouldn't

have any problem at all oscillating at 200kHz.

 

I've chosen a Colpitts type circuit for the frequency-selective network. This incorporates an LC tuned circuit with

the capacitor split to provide a tap for the feedback. Whether that's a good choice, I don't know. An alternative

arrangement would be to split the inductor (that one's called a Hartley oscillator), but the Colpitts seemed

simpler. There's also a further variation on the Colpitts called a Clapp oscillator; I might take a look at that

one in a subsequent blog.

 

The Circuit

 

I haven't designed this from scratch myself, instead I based it on a circuit that I had previously spotted

somewhere. I could remember the circuit shape but not any of the component values. My choices might not be very

good ones.

 

Here is the general form of it

 

image

The JFET in that circuit is set up as a common-gate amplifier. That means that the gate terminal is common to both

the input and the output signals (one of the terminals has to be common to both input and output because the device

only has three terminals). The input is applied to the source terminal and the output is taken from the drain

terminal. If you're only used to the common-source [or common-emitter for a BJT] configuration it will look a bit

odd, but it's a perfectly valid way to use the device. When we talk about configurations like this (common-source,

common-gate, or source-follower), we're talking about circuit configurations and, more specifically, how ac signals

see the circuit. The active device itself just works the way it always works, it doesn't work in a different way

for each configuration, and we need to make sure that the dc biasing, necessary for it to operate at all, functions

properly, irrespective of how the ac signals view matters.

 

In this circuit, the LC circuit forms the output load at the drain. Because current needs to run down through the

JFET to bias it correctly, the load goes up to the rail rather than down to ground. To an ac signal, the rail can

be considered as more or less the same thing as ground: at higher frequencies, the decoupling capacitors should

look much like a short circuit between the two. It also satisfies the dc conditions because, at start-up, even

before the oscillation gets going, drain current has a path through the coil.

 

The resistor from the source to ground sets the bias point of the device. Arranged like this, the JFET self-biases.

It looks a bit odd on a circuit, but once you understand it it's quite straightforward.

 

Here it is in the simulator

 

imageimage

 

With zero ohms, the current is the Idss value. The simulator thinks that it is about 8mA. That's reasonably close

to the values I get with my bag of JFETs which are something like 9mA. With 470R, it's just over 2mA, giving a

voltage at the source of around 1V. I decided to go with that for the circuit. I can live with 1V at the source and

2mA is a reasonable figure for the standing current. It might not be obvious, but the JFET regulates that current,

and hence the voltage at the source. If it increases, the voltage between source and ground increases and then the

gate going more negative (relative to the source) has the effect of reducing the current. If it decreases, the

voltage between source and ground declines, the gate is relatively less negative, and the current will increase.

 

A consequence of using the common-gate configuration and having that resistor there at the input is that it becomes

the input resistance and, since it will only be a few hundred ohms, that makes it a fairly low input resistance for

an amplifier.

 

When choosing the L and the C, I have a choice as to the values. As I want to be able to change the frequency quite

significantly, maybe by about 5% from the nominal frequency with just a comparatively small amount of additional

capacitance, I need to keep the capacitance fairly low and go for a higher value coil to get the frequency I want.

I've got some 470pF capacitors, so I can have two in series for the capacitor side, giving a capacitance of 235pF.

If I put those together with a 2.2mH inductor, the resonant frequency is going to be 221kHz, which is about where I

want it. That frequency won't be the exact frequency of oscillation for a couple of reasons. One is additional

circuit parasitic capacitances and inductances that I'm not taking into account. Another is that the oscillation

won't take place at exactly the point where the tuned circuit looks real, and introduces no phase shift, because

the criteria is for the full loop and not simply the tuned circuit.

 

The Breadboard

 

Here it is, thrown together quickly on a breadboard:

 

image

 

Fortunately, it does actually oscillate. The yellow trace is the signal at the drain of the JFET. The blue trace is

the signal at the source.

 

image

 

But it's noticeable, even just looking at the trace, that the output isn't a very good sinewave [look at the bottom

of the yellow trace, where it starts to come back up again, and you can see how it is misshapen]. If I look at it

as an FFT on the oscilloscope I can get an idea of the extent of the distortion:

 

image

 

As well as the fundamental, we also have ALL the harmonics in declining proportion. As a THD [Total Harmonic

Distortion] figure, that would easily be several percent. I can see two reasons for that. One is that we're

operating the JFET with a large signal and suffering from the non-linearity that comes from the gm [forward

transconductance] varying as the bias point of the transistor moves around. The other is down to the crude way the

waveform limits.

 

Time-wise, it's moderately stable - better than I would have expected for something so simple. If I trigger on it

and then look at the next point where it has the same amplitude as the trigger point, one cycle on from the

trigger, I see a variation of about plus or minus 1ns.

 

image

 

Here's how it behaves at start-up:

 

image

 

the yellow trace is the signal at the drain, the blue trace is the voltage from the bench power supply as it comes

up. It always seems to start reliably; I haven't had it fail yet. (Don't worry that the yellow trace looks a bit of

a mess in the picture: that's simply aliasing in the way that the 'scope presents the display. The overall envelope

that the trace shows will be fairly accurate.) Incidentally, that trace emphasises how, because of the tuned,

resonant circuit, the drain waveform climbs above the power rail.

 

Looking at the Circuit in the Simulator

 

Here I'm simulating the circuit in TI-TINA. These are the equivalent waveforms to the oscilloscope ones above.

 

image

the shapes are similar, but there is some difference. I would imagine that's mostly the difference between the JFET

model and the real device.

 

If I put an ammeter in series with the drain on the simulation, we can immediately see how the distortion arises

 

image

This is a somewhat non-linear circuit, with the JFET sending pulses of current to the tuned circuit. Potentially, that

could be a good thing. Apparently, for good waveform shape and low phase noise, a good approach is to let the tuned

circuit do all the work and just give it a short nudge, once a cycle, away from the important timing points, a bit

like gently pushing a child's swing at the top of the arc. In this case, though, it's more like intercepting the

swing before it reaches the top and forcefully sending it back.

 

Opening the Loop

 

To understand better how the circuit behaves (in a simulator, so only as good as the models involved), one approach

I have is to open the loop. This won't be simulating the breadboard circuit at all accurately because the physical

circuit is working with very large signals whereas the simulation will be working small-signal and won't be seeing

the large-signal distortion, but for all that it might show some useful things to us.

 

Here's the circuit. You can see I've added two additional components, a capacitor and an inductor, and two test

items, a voltage generator to provide a swept input and a voltmeter to record the output.

 

image

The two added components don't affect the way the circuit operates, instead they allow us to trick the simulator.

For DC, the simulator will calculate the operating points as though the loop were closed, for AC, the simulator

will then give the response as though the loop were open.

 

Here is the Bode plot I get:

 

image

That shows us a nice sharp resonance at a couple of hundred kilohertz and a softer antiresonance at a much lower

frequency that isn't of much consequence because there's no loop gain there. The LC circuit is responsible for the

resonance peak at just over 200kHz. At that point the phase abruptly changes, passing through zero as the LC

circuit changes from looking inductive to capacitive. That gives us our two criteria for oscillation, a frequency

where the phase shift can settle to zero and where there is also gain of more than one so that the oscillation is

sustained (ie at or above 0dB on the gain graph). The rapid way the phase changes shows why an LC tuned circuit

like this is good at determining an oscillator frequency.

 

Here is a more detailed view

 

image

 

That's reasonably close to where the oscillation frequency actually was. It's also useful because it appears to

show that there isn't too much likelihood of the circuit oscillating at the wrong frequency because of the way the

gain falls off away from the resonance point. [I have to be careful here because, as I said, I'm not simulating the

large-signal oscillation of the actual circuit. Also, JFET parameters vary widely between different batches of the

parts, so the typical figures in the simulator's model might not be very close to the actual devices I've got.]

 

Conclusions

 

I ended up with something that oscillates, it starts reasonably well, and it seems fairly stable. The waveform

isn't anything to write home about - quite a poor sinewave - but, given the very small number of components, I

don't suppose I should complain too much about that. [Actually, I was a bit surprised that it worked as well as it

did.]

 

If you found this interesting and would like to see other blogs I've written, a list can be found here: jc2048 Blog Index

  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +3
    I remember doing Colpitts oscillators back in tech school. Of course in those days, we built our circuits using triodes because the new fangled semiconductors were still too expensive. We studied JFET…
  • vasista333
    vasista333 over 5 years ago +1
    hello good day i am also working on JFET colpitts oscillator and i am trying to define my nano-mechanical transistor using JFET colpitts oscillator, i read the paper and i am trying to to the frequency…
Parents
  • vasista333
    vasista333 over 5 years ago

    hello good day i am also working on JFET colpitts oscillator and i am trying to define my nano-mechanical transistor using JFET colpitts oscillator, i read the paper and i am trying to to the frequency of 80 khz- 10Mhz of freqeuncy, could you help more in detail about this any help could be appreciated.

    thank you

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vasista333
    vasista333 over 5 years ago

    hello good day i am also working on JFET colpitts oscillator and i am trying to define my nano-mechanical transistor using JFET colpitts oscillator, i read the paper and i am trying to to the frequency of 80 khz- 10Mhz of freqeuncy, could you help more in detail about this any help could be appreciated.

    thank you

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 5 years ago in reply to vasista333

    I don't understand quite what you're asking. I've never heard of a nano-mechanical transistor.

     

    There's the start of a proper theoretical treatment (and further references) on the Wikipedia page, if that's what interests you

     

    https://en.wikipedia.org/wiki/Colpitts_oscillator

     

    Colpitts oscillators (and variations like the Clapp oscillator, and others involving different configurations of the reactive feedback components like the Pierce and Hartley) were, at one time, used extensively in radio design for local oscillators, so you should find an extensive literature on them if you have access to a good academic library (or even just some old radio engineering books).

     

    This blog was just me spending an afternoon playing with a JFET and seeing if I could make something work without designing it properly from theory, merely by slapping components together.