Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Just Finished My Python Course : Can you run Pythin directly on any Arduino?
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 21 Feb 2020 12:17 PM Date Created
  • Views 2499 views
  • Likes 8 likes
  • Comments 23 comments
  • python
  • arduino
Related
Recommended

Just Finished My Python Course : Can you run Pythin directly on any Arduino?

dubbie
dubbie
21 Feb 2020

I have just finished my Introduction to Python Course put on by FutureLearn which was not too difficult and I think I might have learnt something. Now I want to try out a few things - I still do not know how to blink a LED in Python yet.

 

What I would like to do is to run Python programmes (scripts?) directly on an Arduino. I have looked on Google and so far I have not found anything that indicates it might be possible. I know that Python is interpreted but does anyone know if there is a powerful enough Arduino that has had Python ported to it? I know the Raspberry has and probably other boards as well.

 

Dubbie

 

PS My Java course, also on FutureLearn started this week, hopefully learning two languages in such a short time will not be too confusing.

  • Sign in to reply

Top Comments

  • tariq.ahmad
    tariq.ahmad over 6 years ago +4
    Hi dubbie , I don't have an exact date but I know this will be a pretty big deal when its released: Arduino Portenta H7 Powered by STM32H7 Supports Python and Javascript Out of the Box! We will be carrying…
  • michaelkellett
    michaelkellett over 6 years ago in reply to dixonselvan +3
    It takes a while to get to the point but your link is about running Python on a PC and it talking to an Arduino: However, there are some approaches you can take to use Arduino with Python or other languages…
  • beacon_dave
    beacon_dave over 6 years ago +3
    You may be able to install CircuitPython on some Arduino boards based on the SAMD microcontrollers. https://learn.adafruit.com/installing-circuitpython-on-samd21-boards Some examples of digital IO here…
  • tariq.ahmad
    tariq.ahmad over 6 years ago

    Hi dubbie ,

     

    I don't have an exact date but I know this will be a pretty big deal when its released:

     

    Arduino Portenta H7 Powered by STM32H7 Supports Python and Javascript Out of the Box!

     

    We will be carrying the board and will have community activity around it to support its release.   It's something I'm really excited about and something I could see you digging, especially for its robotics applications.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago

    Hi Dubbie,

     

    I know this isn't answering your specific question, but I was wondering if you have access to a Pi. If so, it's a very nice way to get familiar with I/O with Python, because you've the got access to normal Python, plus any libraries you want/need.

     

    To do input/output, some library is needed with the Pi. A popular one is gpiozero (although personally I don't like it, it's tutorials use a way that totally abstracts away physical I/O and replaces with pre-created classes for specific components. For example, there's an LED class and so on).

    An alternative easier-to-understand I/O library just provides I/O and nothing else - that's RPi.GPIO library, and using it is similar to using a microcontroller, in that a value is set to define input or output mode, and then True or False is set to turn an output on or off.

    There's an example pasted below, taken from Raspberry Pi GPIO Explained

    For Arduino, I think today most examples will still be in Arduino language (i.e. C pretty much) which is no bad thing, because C is used with nearly all microcontrollers, so still worth learning that too. Again, sorry for not directly answering your question, I've never used Python on an Arduino, perhaps I'm missing out.

     

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to beacon_dave

    I'd missed that one - Circuit Python isn't complete actual Python but it does have the compiler running on the micro so it may well do what Dubbie wants.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 6 years ago

    Does it have to be an Arduino? If you've got a micro:bit, you could try programming that with MicroPython. That's in the same sort of price area as one of the simpler Arduino boards and has a reasonable amount of IO to play with. It's not the full language, but would be fine for control type stuff.

     

    https://microbit.org/code/ (see link to editor partway down page)

     

    https://www.python.org/community/microbit/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago

    You may be able to install CircuitPython on some Arduino boards based on the SAMD microcontrollers.

    https://learn.adafruit.com/installing-circuitpython-on-samd21-boards

     

    Some examples of digital IO here:

    https://learn.adafruit.com/arduino-to-circuitpython/digital-in-out

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>